Americas
Products
Service
Solutions
Resources
Support
News & Events
About Us
MELSEC iQ-R Series: As the core for next-generation automation environments, Mitsubishi Electric has created an automation controller with added value while reducing TCO.
The MELSEC iQ-R Series has been developed from the ground up rationalizing common problems into seven key areas: Productivity, Engineering, Maintenance, Quality, Connectivity, Security and Compatibility. It uses a three-point approach to solving these problems: Reducing TCO, increasing Reliability and Reuse of existing assets.
iQ-R Series Overview
iQ-R Series Selection Tool
Programmable automation controllers catering for various applications.
The base units are needed for installing devices such as power supply, CPU and I/O modules. Various types are available to suit multiple system requirements.
This module is used for providing the electrical power for the CPU, input, output, and other modules on the base unit.
Devices such as switches, indicator lamps, and sensors can be easily connected to the control system using the digital I/O modules.
Analog modules are the main interface between the control process and the automation system and are specifically designed to interface with sensors that process varying voltage and current signals.
Distinct set of high-accuracy, fast and intelligent control response modules that are ideal for applications requiring high speed and precision.
This module group enables information exchange with multiple control systems. The module lineup improves production efficiency by collecting and controlling various production information.