The system has been designed for users currently using or considering use of Mitsubishi Electric products.
The system can be used as reference models for configuring a MELSERVO system. Please refer to catalogs and manuals relevant to configurations obtained by the model selection tool.
We do not take any responsibility for any damage or loss caused through use of the system.
The software includes open source software licensed under MIT License, SIL OFL 1.1, and CC BY 3.0. For more information about open source software, please refer to the list and the license in the link below. If there is a conflict between the contents of open source software license and the terms of use, the open source software license will control. About open source software license
Notes
The copyright of the software is possessed by Mitsubishi Electric Corporation and licensors of each open source software.
The contents in the system may be deleted or changed without prior notice.
There is no guarantee about upward compatibility of data in the system (Previously saved data may not be compatible with the new system version).
The system has been confirmed to work on the following browsers: Microsoft Edge, Internet Explorer 11, and Google Chrome.