Ready to Order?

ICONICS Suite Order Form

Stay Informed
FacebookNew44 LinkedInNew44 X244x44 YouTubeNew44 InstagramNew44 Blogicon2

SCADA software-ICONICS Suite™

Ready to maximize your system performance? Request a Quote Contact Sales


What are tags?

Tags are data sets for GENESIS64™ to access external devices. The number of data sets used in runtime of GENESIS64™ are counted. In the example below, a device value of a programmable controller = 25 and an SQL statement that refers to the last week temperature data are targets counted.

What are tags?

In the case of Hyper Historian™

  • When using Hyper Historian™, tags are counted separately from GENESIS64™*1*2
  • “The number of historical data collection settings” are counted as the number of tags

Difference of counted tag

Type of data Real-time data Historical data
When using Hyper Historian™ GENESIS64™ tag Hyper Historian™ tag
When using Hyper Historian™ Express GENESIS64™ tag GENESIS64™ tag
*1. When using historical data collection/accumulation (Hyper Historian™ Express) included in GENESIS64™ server product, a tag is counted as GENESIS64™ tag.
*2. Historical data collection setting that exceeds the number of tags of Hyper Historian™ in use cannot be counted as GENESIS64™ tag.

In the case of Hyper Historian™