Americas
Products
Service
Solutions
Resources
Support
News & Events
About Us
New white paper, Maximize Machine Vision Guided Robotics, discusses 2D and 3D vision for prospective and existing users. Download Now
Prepared the option for further advanced applications. By utilizing such as high precision vision sensors or force sensor, it can automate the advanced work that couldn't be done until now.
The R86TB is a new teaching box further evolved from the conventional high-performance teaching box. Even if a computer cannot be brought to the site, one teaching box can handle a series of processes from setup to maintenance, reducing time and cost.
The vision sensor is developed exclusively for use with Mitsubishi Electric FA devices and offers better compatibility with them.
Operators can enter to the robot operation area without stopping the robot system.
The AnyWire ASLINK wiring system can be incorporated in MELFA robots, to resolve gripper wiring problems.
The multifunctional electric hand option supports customer's various applications with various functions, great lineup, and highly accurate gripping.
Allows copy and fitting work to be completed in the same way a person would while the force applied to the hand is monitored. Enables necessary work such as fine force adjustments and force detection to be completed.
More Information