Supplier Open Bid Announcements
MELCO HVAC US, Inc. ("MEHVAC") is soliciting suppliers to provide products and services in support of its Inflation Reduction Act (IRA) Maysville High-Efficiency Heat Pump Compressor Manufacturing Project (the "Project"). As part of the Project, MEHVAC will be retrofitting its Maysville facility to create the capacity to manufacture up to 1 million twin-rotary variable speed capacity compressors annually. MEHVAC actively is seeking partners to help!
In the first phase of the Project, MEHVAC will focus on procuring the necessary resources to retrofit and redesign the facility. Over the next nine months, MEHVAC will issue formal requests for competitive proposals (RFPs) for the products and services we need. As the Project is being funded in part by the U.S. Federal Government, these solicitations will follow the Federal procurement method used for the acquisition of goods and services with federal funds per Uniform Guidance 2 CFR 200.320(b)(2). MEHVAC particularly welcomes proposals from U.S. companies, as well as small and diverse suppliers!
If you are interested in providing products and services in support of the Project, please click on the following link to review the open solicitations.