UPS
BETTER DOESN’T HAVE TO MEAN BIGGER.
Our uninterruptible power supply (UPS) systems deliver exceptional power density, quality, reliability and efficiency. They exhibit technical excellence while occupying minimal floorspace.
Whether it be in support of IT, communications, medical or manufacturing equipment, Mitsubishi Electric has a UPS designed for continuous power to be supplied and critical operations are not interrupted.
UPS COMMON PROBLEMS, UNCOMMON SOLUTIONS
>99.9993% uptime
DOWNTIME
If downtime equals disaster for your business, then it makes sense to partner with someone that can deliver the most uptime. Mitsubishi Electric delivers reliability among backup power equipment suppliers through robust proprietary technology designed to deliver continuous power in demanding environments. Mitsubishi Electric’s installed base of 9900, 1100, and Summit Series uninterruptible power supplies have sustained load-carrying capability during more than 99% of their actual operational history. That’s power you can depend on.
Up to 99%
HIGH EFFICIENCY
Efficiency reduces energy costs and significantly impacts a data center’s bottom line. Mitsubishi Electric’s proprietary double-conversion technology delivers this efficiency without compromising load and power protection. Mitsubishi Electric’s SUMMIT Series® UPS holds the number-one rating on the Energy Star® website in the AC-Double Conversion (VFI) product category.
PERFORMANCE
ULTIMATE CONTROL
The key to achieving optimum UPS performance is insulated-gate bipolar transistor (IGBT) power device control. Utilizing a combination of high sampling rates and direct digital control (DDC), Mitsubishi Electric UPS systems are able to perform under severe load conditions. Resulting benefits include excellent output voltage control, dynamic inverter response and minimal voltage distortion during full load steps without the DC source. This maximizes the performance of the UPS and increase the overall reliability of components and the system.
UPS SYSTEMS THAT PROTECT
RELIABLE, SPACE-SAVING AND ENERGY EFFICIENT
As the cost of downtime continues to climb, Mitsubishi Electric achieves some of the highest levels of reliability among backup power electronic suppliers. In addition to maximizing uptime, Mitsubishi Electric delivers critical power solutions that provide excellent value in the areas of high efficiency, rapid deployment, total cost of ownership, scalability, premier service and support.
9900 AEGIS™ SERIES
The 9900 AEGIS™ is the smallest in the popular 9900 Series UPS line. The AEGIS is a three-phase, online double-conversion system and features Mitsubishi Electric’s acclaimed three-level IGBT technology for enhanced performance and reliability. The AEGIS boasts a relatively flat efficiency curve, indicating that it is highly efficient regardless of the load.
9900B SERIES
The 9900B series delivers as much as 97% system efficiency at unity power factor, substantially reducing operation and cooling costs by thousands of dollars annually when compared to the competition.
SUMMIT SERIES
Certified by Energy Star® in September 2017 to demonstrate 99% efficiency, the Summit Series UPS is rated as the most efficient online UPS. Mitsubishi Electric continues to lead the critical power equipment industry by introducing the first UPS to feature silicon carbide (SiC), the technology described in proceedings of the IEEE as a revolution in power electronics.
DIAMONDPLUS® 1100 SERIES (1100A AND 1100B)
With the DiamondPlus® 1100 Series UPS system, Mitsubishi Electric quality and reliability extend beyond the utility power room. Perfect for server rooms, network closets and control rooms, DiamondPlus models provide high-performance power protection for lower but still critical loads.
MITSUBISHI ELECTRIC: AT THE FOREFRONT OF INGENUITY AND INNOVATION
Want to know what makes Mitsubishi Electric UPS so efficient? Watch this video.
See how Power Devices are used to power our products.
WHITE PAPERS
Building for Efficiency: Systems Approaches Boost Profitability


Owners and developers deploy building system solutions—including vertical transportation, HVAC and UPS—leveraging impr...
Silicon Carbide-Based Uninterruptible Power Supplies


When it comes to energy requirements for today’s data centers, we find that there are ever-increasing needs to be able ...
The Payoff of Preventive Maintenance


The UPS is the most critical component in protecting the integrity of your data, regardless of whether it’s merely prov...
ARTICLES
The Power of Understanding Uninterruptible Power Supply Systems


Going dark is a potential disaster for tenants and business owners alike. When constructing more efficient buildings for...
Minimizing Downtime in Critical Power Infrastructure
The following information provides a general guideline in the design, implementation and operation of your critical powe...
CASE STUDIES
DataChambers and the 9900B Series UPS System
When a competitor’s uninterruptible power supply (UPS) didn’t live up to expectations, DataChambers needed to replace ...
Case Study: Sky High Customer Service
When ViaWest needed a reliable UPS system for their 22 data centers and 13 network operations centers, they looked to Mi...