Americas
Products
Service
Solutions
Resources
Support
News & Events
About Us
Network Software Tools Provide an Improved CNC Environment.
Development Tools : Design & Setup User Support Tools : Training & Oparation Support
Allows the OEM the ability to determine the optimal servomotors for the machines needs by selecting the machine configuration and inputting the machine specifications.
This software tool provides the ability to create original custom screens to your CNC.
NC Trainer2 /Trainer 2 plus provides an application for the engineer to learn how to operate the CNC screens and check machining programs on a Computer without using the CNC Control unit or a special display unit.
The NC Data File necessary for NC Control and Machine Operation (Such as parameters, Tool Data and Common Variables) can be edited on a personnel computer.
You can automatically adjust the servo parameters by running the axes using machining programs. The parameters will adjust by the software measuring and analyzing the machine characteristics.
CNC machining data files can be shared between machines by connecting the NC to a host PC via EtherNet connection.
NC Monitor 2 software allow you to take advantage of the network in the plant. CNC operation status can be monitored from a remote location.
An identical NC display screen can be displayed on a personal computer. By connecting a personal computer to the NC unit when necessary, various data can be checked and set using the same HMI as the standard NC screen.