System Configuration
The Motion module can function as a master station of CC-Link IE TSN.*1
This feature enables users to create a system more flexibly by connecting various devices, such as servo amplifiers, remote I/O modules, and TCP/IP devices, to the Motion module.
![System Configuration](-/media/88563d74f6ce4c0a9ed7c8f7cf39e8ad.ashx?h=796&w=688)
- *1. The Motion modules are not provided with the following functions: sub-master station, local station, multi-master configuration, and backup/restore function.
- *2. Standard stations refer to slave stations other than motion control stations on CC-Link IE TSN. TCP/IP devices are not included in the standard stations.