fa_logo

Educational Resources

CNC Simulators

mini_hero_banner
Information regarding Mitsubishi Electric CNC based simulators for training students in high schools, colleges and other learning facilities.

Mitsubishi Electric CNC simulators are designed to prepare the next generation of students and workers with the tools they need to succeed in the machining industry. Our simulators provide the ability to develop practical skills in a safe manner. Students utilizing Mitsubishi Electric simulators will be trained on controls and programming methods commonly used by machine tool builders and facilities throughout the world.

M80 CNC Simulator

EDU M80 SIM

M80_CNC_SIM_200x150

Mitsubishi Electric's EDU M80 simulator is a desktop version of the M80 control common throughout the CNC machine industry. This simulator allows students the ability to navigate, program, and simulate milling and turning operations before they are applied to a real machine. The EDU M80 simulator is ideal for new CNC programmers and operators wanting exposure to real-world controls without the risk of physical damage to a machine.


NC TRAINER 2 PLUS SOFTWARE

NC TRAINER_200x150

Mitsubishi Electric's NC TRAINER 2 PLUS SOFTWARE enables students to learn how to program a CNC machine utilizing a laptop computer or PC. NC TRAINER 2 PLUS SOFTWARE is a simulation software that allows theoretical operation of a CNC mill or lathe without the CNC control unit or special display (HMI). This NC Training product is configured with the same software elements one would find on Mitsubishi Electric's state-of-the-art M80 control. NC TRAINER software enables upload or download of programs directly into another Mitsubishi Electric M80 control. Furthermore, this software can be used to educate students in programming, setting tool offsets, feedrates and spindle speeds without the risk of physically damaging a machine tool.