-
Inquiries
-
Select
& Quote -
Share
-
Partners
Programmable Controllers MELSEC-A Series
Renewal
Install the Q Series base unit with the existing installation holes
Upgrade exampleQ Series Large Type Base Unit
Supported series:
Q Series large type base unit (AnS Series size)
The Q Series large type base unit is used to replace the AnS Series module with the Q Series, using the existing installation area and cables.
- Utilizing a 16-point terminal block from the existing AnS/QnAS Series module reduces the rewiring work.
- When replacing the AnS/QnAS Series module with the Q Series by using the conversion adapter (Upgrade tool products by Mitsubishi Electric Engineering Co., Ltd.) and the existing AnS/QnAS Series terminal block without rewiring, the width of I/O slot of this base unit is just the same as the existing wide-sized AnS/QnAS Series, then the space reduces noise interference from nearby modules.*1
- The installation position is the same as the AnS/QnAS Series, and the installation holes can be used to install the Q Series large type base unit.
- Q Series large type base units (AnS Series size) for panel installation and DIN rail installation are available. Select the type for your need.
*1.The Q Series large type blank cover QG69LS (selling separately) is required with the Q Series I/O module.
[Example] Replacing AnS/QnAS Series module with Q Series module using conversion adapters and Q Series large type base unit
- (1)Remove the AnS/QnAS Series module along with the base unit, install the Q Series large type base unit in the same position using the same installation holes, and install the Q Series modules. (No need of making new installation holes when installing the Q Series large type base unit.)
- (2)Attach the Q Series large type blank cover (AnS Series size) to the Q Series module and install the Q Series module to the Q Series large type base unit.
- (3)Attach the conversion adapter (Upgrade tool products) to the Q Series module with the Q Series large type base unit.
- (4)Remove the terminal blocks from the existing AnS/QnAS Series module and attach them to the conversion adapter.
(The existing wiring can be used without modification.*2)
- *2.Partial change in wiring for the power supply and common terminals is required.
- *3.Provided with screw holes for fixing the conversion adapter support flange.
Q Series large type base unit (AnS Series size) list
The following base units are available to use the Q Series modules with the installation holes of the AnS/QnAS Series modules. DIN rail can also be used. The width of I/O slots of this base unit is the same with that of the existing wide-sized AnS/QnAS Series, minimizing the interference from nearby modules.*4
Installation area | Main base unit | Extension base unit |
---|---|---|
Panel surface | Q35BLS Q38BLS |
Q65BLS Q68BLS Q55BLS |
Installation area | Main base unit | Extension base unit |
---|---|---|
DIN rail | Q35BLS-D Q38BLS-D |
Q65BLS-D Q68BLS-D Q55BLS-D |
*4.To install the Q Series module on the I/O slot of the Q Series large type base unit, always attach the Q Series large type blank cover QG69LS (sold separately).