Medical Device
To meet the constant challenges of increasing productivity and rising demand, the medical device industry must be able to adapt to changing requirements. Smaller production areas that operate at higher speeds are prerequisites for state-of-the-art manufacturing facilities. Mitsubishi Electric's integrated automation technologies provide the greatest flexibility in today's production environments. The benefits in the manufacture of medical devices are illustrated best through real-world examples.
Our robots offer high speed, high accuracy and complete traceability. When absolute accuracy is required, such as in the mating of two parts of an artificial joint, our robots can place the joint and measure its precise position in every plane. They can transfer samples to a test station and automatically remove those that don't meet test criteria. Test data is instantly logged and used to provide tracing records. The entirely automated process, which can be run 24/7, ensures that only perfect products advance to packaging.
Ready to connect with Mitsubishi Electric Automation? |
CONTACT US |