fa_logo

Case Study

BW Integrated Systems' Smart Decision Keeps Streamfeeder Innovative

mini_hero_banner
Download PDFPDF
streamfeeder-banner

First Released May, 2021

When parts on BW Integrated Systems’ best-selling Streamfeeder feeding solution were beginning to become obsolete, they looked to Mitsubishi Electric to replace servo and drive components. As they did so, they found that replacing their entire control cabinet with Mitsubishi Electric controls would result in a more versatile and profitable feeder.

A Smart Decision Pays Big Dividends

Streamfeeder, by BW Integrated Systems, is known for their rugged, dependable, and versatile feeding solutions. When the components on their best-selling feeder were being obsoleted, they began looking for servo and PLC replacements.

Their footprint for the new IT 1250 Friction Feeder was pretty small. Paul Swanson, Software Controls Engineer at BW Integrated Systems says, “That’s what got us to make the move to a Mitsubishi Electric servo. They have a lot of compact gear that packs a lot of performance into a small package.” They decided to go with the Mitsubishi Electric MR-J4-B Servo Drive.

Then Tom Schrauth, Senior Sales Engineer at Mitsubishi Electric said, “If the entire control cabinet was Mitsubishi Electric, you’d have a better, smarter, more innovative and profitable feeder.” Paul agreed and BW Integrated Systems decided to go with a Mitsubishi Electric FX5U PLC and HMI too.

streamfeederplc-fx

The Mitsubishi Electric FX5 is the world’s best selling Compact PLC because of its affordable high performance.

Engineered to Deliver More

Because the entire control system is made up of advanced Mitsubishi Electric components, Streamfeeder was able to do more than increase torque and performance. The new feeder also delivers a wealth of new capabilities including:

  • WiFi connectivity – A production manager can be in his office, at home or on the road and still see what's going on with the feeder at any given time. Operators can set-up, adjust and troubleshoot the feeder anywhere on the production line — from a phone, tablet or laptop. That means throughput, downtime and runtime decisions can be made more quickly.
  • Job library – Companies can store job parameters for faster setups. Operators don't have to look up jobs, re-enter parameters or worry about making a mistake. They simply select a job name and push a button. All the job parameters are automatically set from a control standpoint. Paul says, "It's a big time-saver during changeovers."
  • Real-time diagnostics – Management, operators and maintenance personnel can efficiently track productivity, quality and efficiency in real-time. Paul says, "You can open up a report, see how far along the job is and how fast the system is running. Then if all of a sudden, performance drops a bit, you know something’s going on."
  • Preventive maintenance – The system tracks cycles and reminds users to perform specific tasks such as replacing the belts. Maintenance personnel can perform diagnostics and look at performance over the past hour, shift, day or year. The new feeder also makes predictive maintenance attainable in the future because it's a smart machine.
bwfeederquotesmall

The new IT-1250 Friction Feeder is super-fast. Three-to-five cards go through every second. The system is also WiFi-capable.

The decision to do more than simply update the system is paying big dividends. By building it better, Streamfeeder was able to leapfrog the competition. Paul says, "A lot of it wasn't driven by actual market demand now. We’re just trying to look to the future to see where market demand is going."

The next step is collateral control. This will bring error reporting and orchestration to their customers. The goal is to get machines talking to each other. Doug Schulz, National Sales Manager for the Streamfeeder product line says, "This will be a big help to customers who have more than one feeder in their shops."

bluebwintegrated780

“We knew that if we made this all Mitsubishi Electric, we’d have better control of the feeder itself. Interface improvements would increase speed and accuracy and it would be easier to program.”

- Paul Swanson, Software Controls Engineer
BW Integrated Systems

A Crane That Stands Alone

During the re-engineering process Paul Swanson, Software Controls engineer says, "We knew that if we made this all Mitsubishi Electric, we'd have better control of the feeder itself. Interface improvements would increase speed and accuracy and it would be easier to program. We'd also have less holding pressure on the product, which in some cases can leave marks."

Maintenance is streamlined too. Paul says, "Why mix components? If we can get the cost-effectiveness from Mitsubishi Electric, there's no reason not to. Why have such a large inventory of different parts?" Doug says, "We sell equipment all over the world. Because the machine's components are all manufactured by Mitsubishi Electric, they're available all around the world. We know this machine can be supported everywhere we are."

The backward compatibility is huge as well. "We've had other companies we worked with that were constantly changing products on us, so we had to change our design. Mitsubishi Electric has been very good about stabilizing their product line."

BW Integrated Case Study Video

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

melservo-j4-servo-amplifiers

MR-J4-B Servo Drive

MR-J4 family of products leverages cutting edge technology to provide a high functionality, high performance solution with the most flexible amplifier in the Mitsubishi Electric lineup.

fx5-programmable-logic-controller

FX5U PLC + Simple Motion Module

The Mitsubishi Electric MELSEC-F series has undergone many advancements, making way for the next generation MELSEC iQ-F Series, with enhanced high speed bus, expanded built-in functions, advanced SSCNET III/H support, and improved engineering environment with parameter settings in GX Works3 engineering software.

got2000-series-human-machine-interfaces

HMI

GOTs (Graphic Operator Terminals) provide an innovative operation and visualization interface. The growth of your business and the speed of your production depend on many influences out of your control.

streamfeederplc

Streamfeeder Solutions

  • Founded: 1990
  • Business: Streamfeeder is a globally recognized leader in the design and manufacture of innovative automation solutions.

Return to Case Studies