VFD Simulators

MICRO_VFD_SIM_290x215

Mitsubishi Electric's VFD simulators are designed to educate the next generation of students and workers on the fundamentals of inverter technology and the various applications in which they are commonly used. Designed for the classroom environment, Mitsubishi Electric simulators are designed to sit on a desktop and are easily portable. All simulators incorporate an electric motor for the student to realize the effect of their programming efforts. Students utilizing Mitsubishi Electric VFD simulators will learn how to configure and program the VFD and HMI to replicate various constant and variable torque operations common in conveyor, hoist, crane, pump, fan, elevator, and HVAC applications.

MICRO VFD SIM

Designed for the classroom environment, this all-in-one unit easily sits on a desktop. Utilizing built-in keypads, FR-Configurator2, GT-Works3 software and HMI, students will learn to configure and program two independent VFD’s. The FR-D700 inverter is designed for basic low HP general applications, while the FR-E800 is designed to address applications subject to constant or variable torque, and delivers expanded functionality in a compact footprint. This simulator allows the student to program and operate either inverter depending on what the application requirements call for.

MICRO_VFD_SIM_200x150

FR-A800 VFD SIM

Designed for the classroom environment, this unit easily sits on a desktop and is portable. Utilizing a built-in keypad, FR-Configurator2 and GT Works3 software, students will learn to configure and program the VFD and HMI. This is a hands-on demo that allows students to perform the various common and constant torque related operations associated with VFD's. Mitsubishi Electric's FR-A800-E is specifically designed to educate students who are interested in learning programming and functionality capabilities associated with constant torque applications common in conveyor, hoist, crane, elevator and a multitude of other markets.

A800_VFD_SIM_200x150

FR-F800 VFD SIM

Designed for the classroom environment, this unit easily sits on a desktop and is portable. Utilizing a built-in keypad, FR-Configurator2 and GT Works3 software, students will learn to configure and program the VFD and HMI. This is a hands-on demo that allows students to perform the various common operations associated with VFD's. Mitsubishi Electric's FR-F800-E inverter is specifically designed to educate students who are interested in learning programming and functionality capabilities associated with variable torque applications common in pump, fan and HVAC control markets.

A800_VFD_SIM_200x150

FR Configurator2

FR-Configurator2 is a versatile software tool that provides an intuitive interface which saves you valuable application setup and programming time. Users can quickly view and set VFD parameter lists, debug programs, check diagnostics and perform system monitoring functions conveniently from their PC, reducing down time when changes to the VFD are needed.

Frconfigurartor2