Battery Material Data

Periodically, customers have requested material safety data sheets (MSDSs) for batteries supplied with our products. However, under the regulations, MSDSs are not required. Batteries contained in our products are a fully-encased, manufactured item intended as an end-use product for customers. Therefore, batteries are not classified as a hazardous chemical and are not treated as such under the United States OSHA Hazardous Communications Rule. These batteries are considered "articles" within the meaning of 29 CFR Section 1910.1200(c), as they are formed to a specific shape or design during manufacture, have an end-use dependent upon their shape or design, and do not release or otherwise result in exposure to hazardous chemicals under normal conditions of use. Therefore, an MSDS is not required.

However, as a service to our customers, we are providing either manufacturer links or PDF Data Sheets for the following battery types -- Lead Acid, Lithium and Nickel Cadmium which may be found in our products.

In addition, Mitsubishi Electric Automation, Inc. encourages customers to properly recycle all batteries though a local battery recycler. Batteries should not be disposed of with your refuse. Please check with your State or County Solid Waste Agency for the location of recyclers.

Batteries Contained in Mitsubishi Electric Automation, Inc. Products:

Part # - A6BAT, A8BAT, A10BAT, ER6V-C119B - Mitsubishi Electric (Thionyl Chloride) Lithium Cell
Part # - MR-BAT, MR-J2M-BT, MR-J3BAT, MR-J3W03BATSET, MR-J3WBAT, MR-JBAT4, MR-JBAT8, MR-BAT6V1SET(-A), MR-BAT6V1, MR-BAT6V1BJ - Mitsubishi Electric (Thionyl Chloride) Lithium Cell
Part # - GT15-BAT - FDK Corporation (Magnesium Dioxide) Lithium Cell
Part # - BR-C - 3 Volt Panasonic Lithium (Carbon Monofluoride BR type) Cell
Part # - Q6BAT - Mitsubishi Electric (Magnesium Dioxide) Lithium Cell
Part # - Q7BAT - Mitsubishi Electric (Magnesium Dioxide) Lithium Cell Part # - Q2MEM-BAT - Poly-Carbon Monofluoride lithium battery
Part # - Q2MEM-BAT - Poly-Carbon Monofluoride lithium battery
Part # - Q3MEM-BAT - Heat Resistant Coin Type Lithium Manganese Dioxide Battery (CR)
Part # - C52017 - Mitsubishi Electric (Manganese Dioxide) Lithium Cell
Part # - C52010 - Mitsubishi Electric (Manganese Dioxide) Lithium Cell
Part # - C52001/C52100 - Mitsubishi Electric (Thionyl Chloride) Lithium Cell
Part # - FX3U-32BL – http://biz.maxell.com/en/primary_batteries/pdf/CR_psds_16e.pdf
Part # - FX1N-BAT - http://biz.maxell.com/en/primary_batteries/pdf/CR_psds_16e.pdf
Part # - GT11-50BAT - http://biz.maxell.com/en/primary_batteries/pdf/CR_psds_16e.pdf
Part # - FX2NC-32BL, PM-20BL, F2-40BL - http://biz.maxell.com/en/batteries/pdf/ER_psds_16e.pdf