News Center - Press Release
Mitsubishi Electric Automation, Inc. Launches Advanced Anti-Clogging Pump Panel System
FreeFlow is a pre-engineered and fully configurable panel system created for pumping applications where advanced pump control and the need to reduce energy consumption are highly desirable.
Vernon Hills, Illinois - March 28, 2025
Mitsubishi Electric Automation, Inc. has announced its latest pre-engineered solution for pumping applications within water/wastewater, oil and gas, and deep well irrigation industries. FreeFlow is a cost-effective panel solution with advanced pump control capabilities. It is designed to address the challenges of aging infrastructure, frequent pump failures caused by clogs, and the need to reduce energy consumption.
FreeFlow is designed with ease of use, implementation, and superior functionality in mind. It can be built in single or dual-drive configurations, allowing a customer to achieve a tailored, pre-engineered solution. Available, in industry standard horsepower increments of 5HP through 250HP, FreeFlow can be configured with NEMA 3R or NEMA 12 enclosure and has a number of communication and accessory options.
FreeFlow utilizes Mitsubishi Electric's FR-F800 VFD, recognized for its anti-clogging and energy-reducing capabilities and auto-tuning features. These features help to reduce the need for manual declogging of pumps, offering a reduction in energy consumption, and enables faster implementation by reducing programming time. FreeFlow panels also include the GT2500 Series HMI for programming, system data visualization, data logging, troubleshooting, and manual storage. Lastly, FreeFlow utilizes Mitsubishi Electric's FX5 PLC to enable advanced pump control beyond the capabilities offered by the VFD, such as applications that require redundancy and the necessity to switch over to a back-up pump should the main unit fail.
"FreeFlow represents a technology leap in advanced pump control for pre-engineered panel systems. The panel comes standard with a 2-year warranty. The included VFD has an extended warranty of 5 years with Mitsubishi Electric Automation's start-up services," said David Simak, Product Manager (Service), at Mitsubishi Electric Automation.
More Information
- About Mitsubishi Electric Automation, Inc.
Headquartered in Vernon Hills, Ill., Mitsubishi Electric Automation, Inc. is a U.S. affiliate company of Mitsubishi Electric Corporation. It offers a broad product portfolio including programmable automation controllers (PAC), programmable logic controllers (PLC), human machine interfaces (HMI), variable frequency drives (VFD), servo amplifiers and motors, control software, computerized numerical controllers (CNC), motion controllers, robots and low-voltage power distribution products. Additional information about Mitsubishi Electric Automation is available at us.mitsubishielectric.com/fa/en/.
- About Mitsubishi Electric Corporation
With more than 100 years of experience in providing reliable, high-quality products, Mitsubishi Electric Corporation (TOKYO: 6503) is a recognized world leader in the manufacture, marketing, and sales of electrical and electronic equipment used in information processing and communications, space development and satellite communications, consumer electronics, industrial technology, energy, transportation, and building equipment. Mitsubishi Electric enriches society with technology in the spirit of its "Changes for the Better." The company recorded a revenue of 5,521.7 billion yen (U.S.$ 36.8 billion*) in the fiscal year ended March 31, 2025. For more information, please visit .
*U.S. dollar amounts are translated from yen at the rate of ¥150=U.S.$1, the approximate rate on the Tokyo Foreign Exchange Market on March 31, 2025.
- About Mitsubishi Electric Factory Automation Business Group
Offering a vast range of automation and processing technologies, including controllers, drive products, power distribution and control products, electrical discharge machines, laser processing machines, computerized numerical controllers, and industrial robots, Mitsubishi Electric helps bring higher productivity – and quality – to the factory floor. In addition, our extensive networks around the globe provide direct communication and comprehensive support to customers. The global slogan "Automating the World" shows the company's approach to leverage automation for the betterment of society, through the application of advanced technology, sharing know-how and supporting customers as a trusted partner. For more about the story behind "Automating the World" please visit:
- About e-F@ctory
e-F@ctory is Mitsubishi Electric's integrated concept to build reliable and flexible manufacturing systems that enable users to achieve many of their high speed, information driven manufacturing aspirations. Through its partner solution activity, the e-F@ctory Alliance, and its work with open network associations such as The CC-Link Partners Association (CLPA), users can build comprehensive solutions based on a wide ranging "best in class" principle.
In summary, e-F@ctory and the e-F@ctory Alliance enable customers to achieve integrated manufacturing but still retain the ability to choose the most optimal suppliers and solutions.
*e-F@ctory, iQ Platform are trademarks of Mitsubishi Electric Corporation in Japan and other countries.
*Other names and brands may be claimed as the property of others.
*All other trademarks are acknowledged
- Media Contact
Pam Summers
Marketing Communications Manager
Mitsubishi Electric Automation
Pam.Summers@meau.com
+1 (847) 478-2415
-
Inquiries
-
Select
& Quote -
Share
-
Partners