-
Inquiries
-
Select
& Quote -
Share
-
Partners
FR-A800 Series VFDs
SYSTEM SUPPORT (FUNCTION)
- Feature
- Specification
- Standards
- Discontinued
SYSTEM SUPPORT
(FUNCTION)
Numerous functions and the extensive lineup of models are ready to support various systems.
Turn spare VFDs into converters
Changeover between VFD and high power factor converter NEW
Install the FR-A8AVP (option) in a separated converter type VFD to use it as a high power factor converter. To use the converter, the following options are needed: phase detection transformer box, dedicated filter reactor, dedicated reactor for PWM control, dedicated filter capacitor, inrush current limit resistor, etc.
They can be switched to a converter and back to an VFD again to match process requirements.
The converter is classified as the self-excitation three-phase bridge circuit, and achieves K5 (the conversion factor) = 0. The total harmonic distortion of the input current (THDi) is 5% or less*1, which facilitates compliance with the overseas standards related to harmonic suppression.
*1When the input voltage is distorted, harmonic contents increase because power harmonics flow into the converter.
*2FR-A842 VFD serving as a high power factor converter
Reduce the shock caused by switching the power source
Phase-synchronized bypass switching (400 V class only) NEW
The FR-A8AVP (option) and the FR-A8VPB (option) make it possible to detect the phase of the commercial power supply. (For wiring details, refer to page 186.)
By synchronizing the VFD output with the phase of the commercial power supply, the spike in the motor current can be suppressed and shock reduced.
Furthermore, the time required for the switching is reduced, which is more beneficial for larger VFDs.
Without phase-synchronized bypass
With phase-synchronized bypass
Reduced tact time with functionality suited to the application
Anti-sway control NEW
When an object is moved by a crane, swinging at the time of stopping is suppressed on the crane's transverse axis or traveling axis. This control cuts down the tact time and facilitates efficient operation.
Increased magnetic excitation deceleration NEW
Deceleration time can be reduced without a brake resistor.
Tact time can be eliminated at conveyor lines, etc.
Selection of optimum capacity to suit the application
Multiple rating NEW
Rated current and four different overload capacity ratings (SLD rating (super light duty), LD rating (light duty), ND rating (normal duty), HD rating (heavy duty)) can be selected with parameters. The optimum VFD can be selected to suit the application, and by selecting a VFD with SLD or LD rating, equipment size can be reduced when compared with the FR-A700 series. The HD rating is best suited for applications requiring low speed and high torque.
If using a VFD with capacity of 75K or higher, or motor with capacity of 75 kW or higher, always select and install the VFD based on the capacity of the motor with DC reactor.
PLC control with a VFD
Built-in PLC function in a VFD NEW
- Parameters and setting frequency can be changed at the program.
- VFD control such as VFD operations triggered by input signals, signal output based on VFD operation status, and monitor output can be freely customized based on the machine specifications.
- All machines can be controlled by the VFD alone, and control can also be dispersed.
- Time-based operation is possible by using in combination with the real-time clock function (optional LCD operation panel (FR-LU08)).
- The FR-A800-E enables communication between multiple VFDs using the I/O devices and special registers of the PLC function, which can create a small-scale system by Ethernet using the VFD-to-VFD link function.