-
Inquiries
-
Select
& Quote -
Share
-
Partners
FR-XC Series Converter
Application Examples
- Feature
- Specification
- Standards
- Discontinued
Ceiling crane
The regenerative power from the motor is returned the power supply to save energy.
The capacity of the FR-XC series converter is selectable according to the regenerative power of the system, which contributes to space saving.
Printing machines
The regenerative power from the unwinding shaft can be supplied to another VFD, saving the overall energy.
When the harmonic suppression function is enabled, power supply harmonics of VFDs can be suppressed.
Air conditioning of buildings
Power supply harmonics of VFDs can be suppressed, minimizing the effects on other equipment.
Compatibility with networks (RS-485 communication, CC-Link) enables central control of systems in multiple locations. The effects of energy saving can be checked easily.
Conveyor
The regenerated energy of the VFD for the lift application is used by another VFD for the driving application. If there is still an excess, it is returned to the power supply, saving on the energy consumption.
Spinning
As unwinding shafts are driven by a load, operation is always in regenerative driving state.
The regenerative power can be used efficiently by connecting VFDs of other drive shafts to a common bus.
The FR-XC series converter supports the system with more than 6 VFDs (up to 10 VFDs).
Pump (water treatment plant)
Power supply harmonics of VFDs can be suppressed, allowing the compliance with the harmonic suppression guidelines.
The FR-XCB box-type reactor enables wiring reduction as it contains peripheral devices.