fa_logo

VFDs (Inverters-FREQROL) Product Features

Equipment maintenance

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Maintenance timer

The Maintenance timer (Y95) signal is output when the VFD's cumulative energization
time reaches the time period set with the parameter.
A warning is displayed on the operation panel.
This can be used as a guide for when the maintenance of the equipment should be conducted.

〈Applicable models〉

A800 / F800: Three sets of maintenance timer/warning output settings

E800 / D800: One set of maintenance timer/warning output settings

Maintenance timer

Start count monitor

The number of VFD start times is stored in a parameter.
Confirming the starting times can be used to determine the timing of the maintenance, or
can be used as a reference for system inspection or parts replacement.

〈Applicable models〉

A800 / F800

Start count monitor