fa_logo

MELSERVO-J5 Series Servo Amplifier

Concept

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued
Innovate Together

Concept

Create new value with MELSERVO-J5. Unlock performance with a total drive solution.
Maximize system performance

Progressiveness

Progressiveness
For evolution of machines
  • Performance improvement
  • Program standardization

Connectivity

Connectivity
For flexible system
configurations
  • Integration with connectable devices

Usability

Usability
For quick operation start
  • Tool enhancement
  • Improved drive system usability

Maintainability

Maintainability
For prompt detection and
diagnosis of failures
  • Predictive/preventative maintenance
  • Corrective maintenance

Heritage

Heritage
For utilization of existing
devices
  • Interchangeability with previous generation models

Maximize system performance

Click here for details on Motion modules

Product Introduction Movies

Introduction of predictive maintenance by the "Machine Diagnosis Function" equipped in MELSERVO-J5.

Introduction of MELSERVO-J5 compatible servo motor HK series.

Introduction of the newest functions of the MELSERVO-J5 using a demo machine.
The following new functions will be introduced in this video: Increasing maximum torque, Batteryless absolute position encoder, Acceleration/deceleration method, and Cam Number change, Multiple starts.

Introduction of the newest functions of the MELSERVO-J5 using a demo machine. The following new functions will be introduced in this video: Vision system integration, Mark detection, and Cam for rotary knife.

Introduction of the GOT drive using a MELSERVO-J5 demo machine. Solves various challenges at shop floors through interaction of MELSERVO-J5 and GOT2000.

Related Link