fa-logo-black-americas

Blogs

Addressing the Challenges of 5G-Capable Data Center Facilities with Data Center Infrastructure Management (DCIM)

case_study_mini_hero

Discover how 5G technology revolutionizes Data Center Infrastructure Management (DCIM) by driving demand for real-time monitoring, edge computing, and sustainable solutions. This article explores how DCIM tools are evolving to meet the challenges of 5G, ensuring scalability, efficiency, and future readiness in a hyper-connected world.

Addressing the Challenges of 5G-Capable Data Center Facilities with Data Center Infrastructure Management

5G technology refers to the fifth generation of cellular technology, and it has transformed the way that people live their lives, as well as how companies use this technology. There are many benefits to using 5G technology, such as increased connectivity and speed, which outpace the previous generations. With the need for data consumption worldwide becoming more advanced and available at our fingertips, there's a huge demand for real-time services and information. 5G in particular has been able to transform data center infrastructure management heavily since its introduction.

What are the benefits of 5G?

5G is a huge jump from 4G when it comes to data transferring and handling. It is known for its lower latency, increased speeds, and increased device connectivity across the board without compromise. It has become the foundation of new technology that we see today, from artificial intelligence to virtual reality and everything in between.

Why are Data Centers Crucial to 5G Success?

Data centers provide the infrastructure needed to run 5G technology. Because 5G has immense data processing and storage demands, there needs to be an infrastructure that can handle it, which data centers provide. They are ultimately able to support edge computing and massive data volumes, as well as enable real-time applications and network efficiency, and support cloud services, making them critical to 5G development and usage. When this technology was introduced, data centers raced to keep up and build the infrastructure to handle it, which they have. They are now a huge part of why we are able to benefit from 5G today and all the extra technology that comes along with it, such as AR/VR, IoT, and autonomous devices.

How 5G is Shaping Data Centers

Data Center builders and operators implement specific hardware and software solutions to best equip their facilities for 5G systems. Some of these may be small changes, such as increased transmission hardware, or drastic changes such as liquid cooling systems, or even a decentralized approach with more edge computing.

DCIM for 5G Facilities

Beyond hardware considerations, a properly specified DCIM is critical for an efficient system for visibility and cost savings. Decentralized solutions are a great fit for a DCIM system, since an operator can view the health of all the facilities on the same screen. Additionally, having a DCIM solution that has integrated the vast amount of IOT available in the system allows for the most accurate estimate of energy consumption, PUE, and other critical metrics for all concerned parties.

Increased Demand for Computing Capacity

These networks produce a giant amount of data, which data centers process and distribute. Data center computing power must be able to handle the influx of data. This also means that more data centers may be needed and/or an increase in the efficiency of the centers to compute and process more and more information. This presents itself in 5G facilities via liquid cooling systems over traditional HVAC systems, for example. In the future, these facilities will be asked to do even more intense computing, making it critical to have reliable and immediate diagnostics of the hardware's status to prevent failures.

Scalability and Flexibility

Data centers need to be able to scale and stay flexible with the increase in data and workload, especially during high usage times. Data centers must stay sharp and available for this data to ensure that 5G runs smoothly and allows for the data to be shared and transferred instantly with the high connectivity and low latency promise of 5G technology. DCIM technologies are a great way to be adaptable as your Data Center continues to expand or change based on the needs of the 5G network, because adding tags for new connected hardware is a simple process.

Real-Time Monitoring and Automation

This network technology allows data centers to take advantage of having real-time information instantly, as well as automation. 5G allows you to have instant communication between sensors and systems, as well as enhanced automation in power, production, security, and many other areas.

Efficiency and Sustainability

Data centers have long been looked at as an issue for environmental sustainability due to the increase in energy and resources required to keep up with the advanced technology. As 5G continues to skyrocket and showcase immense data transfer possibilities, the concern for its carbon footprint also grows. Data centers, however, can use advanced power management or clean energy sources to reduce their carbon footprint. The ability to take in data from a heterogeneous data center system architecture is the most accurate path towards increased visibility of the system's health and efficiency. Increase your reporting accuracy by using existing hardware by implementing the correct DCIM solution.

Challenges in Infrastructure Upgrades

Data centers must be ready for upgrades and potential challenges that come with using 5G technology. There are a few different challenges that may need to be addressed as we discuss data center infrastructure management.

  • Power and cooling demands due to increased usage and production
  • Integration challenges with existing systems
  • Energy efficiency, sustainability, and the carbon footprint of these data centers
  • Security concerns with increased remote access and increased connection

The Future of DCIM in the 5G Era

Data center infrastructure management in the 5G era has many possibilities in the future, as growth continues. This could look like using automation in data center management to keep up with the growing demand, or using predictive maintenance and artificial intelligence in growth for data centers. Ultimately, IoT, artificial intelligence, data centers, and the use of 5G networking are going to shape the future of data center infrastructure management. With this said, there is a huge importance in developing data management strategies today to keep up with the growing need for more data and more technology within the data centers. This allows them to be prepared for whatever the future has in store for them.

Data Center Infrastructure Management and 5G

Data centers are an essential part of 5G deployment, and it's necessary to have these data centers run this type of technology and network. Because of the growing use of 5G and the growth of technology like artificial intelligence, we can assume that data centers will continue to be crucial to the use of 5G and any other networks that come in the future. With new technology emerging every day, there is the possibility for growth and increased efficiency in DCIM, and the data associated with it. 5G data center infrastructure requires many unique decisions that have to be implemented for the best possible visibility and reliability. A modern Data Center is necessary for a modern method of communication. A safe choice for now and tomorrow, implementing a DCIM solution will provide peace of mind for users and operators of the facility.

Want notifications for new Blogs, White Papers, Case Studies & Webinars?

Return to Blogs