fa_logo

Case Study

Intelligent Automation Means Productivity and Precision

mini_hero_banner
Download PDFPDF

First Released September, 2023

Packaging machinery specialists, Balpack, were approached by a customer seeking an application to cap small bottles precisely and delicately. Balpack found programming expertise with HPE Automation and precision controls utilizing Mitsubishi Electric components.

In every industry, time is money. And in packaging, consistency is king. That's why the packaging world has been moving away from pneumatics and hydraulics to all-digital, electric automation. That's where Balpack comes in.

The professionals at Balpack are known as the Packaging Machinery Specialists. They provide their customers with both standard and custom machinery for packaging everything from food to cosmetics, to nutraceuticals and more.

Give Customers What They Want

A customer came forward asking Balpack for an application that would cap small bottles. They wanted something that could deliver the pre-programmed precision that would easily handle the capping of delicate containers filled with pills, liquids, or powders.

None of Balpack's existing equipment could meet this need, so they decided to build a new machine. To get started, they spoke with their current vendor, who had supply chain issues, was unresponsive, and offered expertise that was less than ideal.

Roman Balcar, Balpack Executive Vice President, said, "If you're not getting value out of a vendor, look for a different one."

So they did. After interviewing several new vendors, they chose HPE Automation, a Mitsubishi Electric Automation Diamond Partner Distributor Elite.

roman-quote

"I have to say that Joe Small at HPE was quite proud of his programs. When we finished the first Star Wheel Capper, we ran it, and I looked at Joe and I said, ‘You know what? I think this is the best machine we ever built. Thank you!"

- Roman Balcar, Executive Vice President
Balpack Inc.

The Right Team Gets It Done

Teams from Balpack and HPE worked hand-in-hand to develop a machine based on a star wheel design, the Star Wheel Capper.

As Joe Small, HPE's Electrical Controls Engineer said, "We recommended going with Mitsubishi Electric Automation through and through. Sometimes, if you have components from several different companies, you get into a quagmire of frustration. Getting it to work together is a pain. But with Mitsubishi Electric, the compatibility is built right in."

With a complete Mitsubishi Electric solution, the development time was shorter. And with HPE, Balpack had a single point of contact to answer every question. Not only was HPE only a phone call away; one of their Subject Matter Experts temporarily rented an apartment down the street from the Balpack facility.

Imagine the Challenge

Picture a powerful machine driven by a world-class VFD and servo. Now picture that machine placing a delicate plastic cap on a small plastic bottle, at a rate of 100 caps per minute. The slightest error in torque or positioning could destroy multiple caps and bottles, or cause the product to leak.

What prevents this? The programming expertise of HPE, and the precision controls from Mitsubishi Electric.

balpackmachine

The Star Wheel Capper is the result of a great collaboration between teams from Balpack Inc. and HPE Automation, a Mitsubishi Electric Automation Diamond Partner Distributor Elite

Easy Configuration

"We ran all Ethernet-based controls for our VFDs," said Brian Hord, HPE President and Co-Owner. "That gave us easy configuration and adjustability. We also ran the SMC valves via Ethernet for ease of setup. In the past, the wiring time was considerable. Now they just plug in RJ45 cables."

And according to HPE's Automation Sales and Technical Products Manager, Jason Schmidt, "In older machines with analog controls, you could get only 16 speeds for torque. Now, the number of speeds is unlimited. And torque control is adjustable to one tenth of one percent."

Settings and Changeovers: Quick and Simple

To make new settings easy, HPE worked with Balpack's control engineer to make programming uncomplicated. To create a new setting, the operator simply positions everything as needed, then presses the button marked SET.

"It's a very operator-friendly machine," said Roman Balcar. "And HPE provided the training, which enabled our Balpack operators to do the programming."

caroline-quote

"The most important thing to me is the relationship with HPE. I worked very closely with their team on everything...just having that relationship and a vendor I can lean into is amazing."

- Caroline Shipp, General Manager
Balpack Inc.

A Friendly Interface

All settings can easily be controlled through a user-friendly HMI from Mitsubishi Electric. And recalling those recipe-driven settings for changeovers is even easier. In the past, changeovers were often done manually with an Allen wrench. The process could lead to significant downtime. But with the system's digital controls and Ethernet connections, changeovers can be done in minutes.

By consulting with HPE and Mitsubishi Electric, Balpack has been able to build a capping machine that not only delivers as promised, but can be assembled and running – not in two weeks, but in two days.

Caroline Shipp, Balpack General Manager, valued the partnership that was created. "The most important thing to me is the relationship with HPE. I worked very closely with their team on everything: timelines, availability of products, programming, and how we can stock for the future. Just having that relationship and a vendor I can lean into is amazing."

Roman stated, "And the value that Mitsubishi Electric brought to Balpack allowed us to give our customers a lot of bang for the buck."

Coming Soon

Caroline added, "Mitsubishi Electric was literally the savior of this project. They got us what we needed, when we needed it. Plus, they were open about pricing. That's important for a company of our size." Balpack customers have been asking for a dual function machine that can not only cap but fill. And when it comes to the development of Balpack's new Monoblock system, HPE and Mitsubishi Electric will be ready to assist.

Balpack Case Study Video

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

fx5-programmable-logic-controller

FX5 PLCs

The Mitsubishi Electric MELSEC-F series has undergone many advancements, making way for the next generation MELSEC iQ-F Series, with enhanced high speed bus, expanded built-in functions, advanced SSCNET III/H support, and improved engineering environment with parameter settings in GX Works3 engineering software.

melservo-j4-servo-amplifiers

MR-J4 Series Servo Motor & Amplifier

MR-J4 family of products leverages cutting edge technology to provide a high functionality, high performance solution with the most flexible amplifier in the Mitsubishi Electric lineup.

mr-je-servo-amplifier

MR-JE Servo Amplifier

MR-JE family of products leverages advanced functionality such as true one-touch auto-tuning, vibration suppression, and machine diagnosis functionality in an easy-to-use servo solution.

fr-e800-variable-frequency-drives

FR-E800 Series VFD

The FR-E800 Series variable frequency drive is built upon Mitsubishi Electric’s proven variable speed control technology throughout years of reliable operation across various constant and variable torque applications.

fr-d700-variable-frequency-drives

FR-D700 Inverter

FR-D700 is Mitsubishi Electric’s class-leading range of micro drives. Suitable for a wide variety of general purpose motor speed control applications, the FR-D700 was built from the ground up using custom components and has earned an enviable reputation for durability and dependability in adverse environments.

GOT-2000-Series-GS2107-WTBD-HMI-display-unit

GS2107 HMI

GOTs (Graphic Operator Terminals) provide an innovative operation and visualization interface. The growth of your business and the speed of your production depend on many influences out of your control.

balpack-logo-large

Balpack Inc.

  • Founded: 2000
  • Business: Balpack Inc. provides standard and custom solutions from stand-alone semi-automatic machines to fully integrated automatic packaging lines.

hpelogo

HPE Automation

  • Founded: 1980
  • Business: HPE is the largest distributor for SMC Pneumatics in Florida and the oldest SMC distributor in the United States.

Return to Case Studies