fa_logo

Case Study

JR Machine Uses Automation to Produce More, With Limited Space

mini_hero_banner
Download PDFPDF
jr-machine-banner

First Released December, 2021

JR Machine had reached the limits of their production capacity. Space constraints in their manufacturing facility made physical expansion impossible, so they turned to automation to improve efficiency and reduce downtime. Integrating Mitsubishi Electric M700 CNC controls into their multitasking lathes helped the company dramatically reduce setup and cycle times.

Breaking Through Capacity Constraints

JR Machine is a leading, ISO-certified contract manufacturer for OEM and tier one/two manufacturers. Precision turning with live tooling is a core competency. The shop takes on jobs in the range of 1 to 10 inches in diameter and as much as 28" in length. Customers include some of the biggest and best-known names in the fields of defense, medical, machinery, hydraulics, oil and gas and even auto racing.

A few years ago, JR hit a capacity wall. They couldn't put any more equipment in the building and couldn't expand the building. Their backlog of jobs forced them to run 24/7 with two 12-hour shifts. The only way to increase capacity was to improve productivity. The goal was to eliminate 4,000 hours per year of inefficient production time.

Workpiece transfers are often the biggest contributors to unproductive machining time, because the machine has to stop while operators load and unload parts. JR Machine decided to eliminate this inefficient time by automating transfers using a series of spindles.

JR Machine

To improve performance and accuracy, JR Machine standardized on DMG MORI machines with Mitsubishi Electric CNC controls.

To facilitate the automation, JR Machine installed DMG MORI NLX 2500 Series sub-spindle multitasking lathes with top-of-the-line Mitsubishi Electric M700 CNC controls. The machines have part-catching and part-conveying capabilities. These capabilities along with the controls give Tim and his team the ability to machine a part in a single setup. They no longer have to manually unload and then flip the part or complete the second side in a separate operation. This has reduced setup time and cycle time.

Integrating these machines into their shop had an immediate impact on high volume jobs. Tim Tumanic, President of JR Machine says these new features give them much better machine performance and varying degrees of higher uptime. On some projects, uptime increased by 30 percent in comparison to older models. The machines also enable long stretches of unattended operation. In one case, a job ran over an entire weekend, only requiring an operator to come in two hours each day to check on the two machines.

Machine Bay

Automated parts transfers and improved machine performance have enabled lights out operations and increased uptime by up to 30%.

Standardizing On One Control Platform for Rock-Solid Reliability and Durability

Several years ago, JR Machine decided to work exclusively with DMG MORI. Tim says, "The Mitsubishi Electric control was a pretty substantial part of that decision. Previously, when we used controls from a different company, we had lots of revisions and technicians coming into the shop. Now we don't have that. It's a real positive experience. I don't have to think about the controls at all."

One of the things Tim likes most about the Mitsubishi Electric M700 CNC controls is their rock-solid reliability and durability.

Tim says the move to standardization brings value on many levels. It's easier for them to:

  • Redeploy people to different machines, because the machines and work centers are the same
  • Get newly purchased machines online quickly, because they are tooled just like the others
  • Roll out continuous improvement initiatives, because the shop only has to focus on one machine platform

Standardizing on one control platform also makes scheduling easier, because jobs can run on virtually any machine.

Tim Quote

“They run so flawlessly, none of our operators have ever had to go back into the control parameters or order additional parts. Across 26 machines, you would think something would have come up, but there’s never been any issues—none at all.”

Tim Tumanic, President
JR Machine

Getting More Parts Out the Door More Affordably

The machines have delivered huge cost savings for their customers and decreased lead times too. Tim says, "We're committed to growing with the OEMs and tier one/two manufacturers we serve. We will continue to embrace new technology that improves precision and quality and allows for greater efficiencies in our operations."

This 'continuous improvement' mindset has resulted in significant business growth for the company and industry recognition for Tim. In 2018, JR Machine won Wisconsin's "Manufacturer of the Year" among companies with less than 100 employees.

When asked about the future of machining at JR Machine Tim says, "We see more automation." Tim is considering adding machine-loading robots between pairs of turning centers. This might make it possible for one machinist to tend four machines.

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

m700-series-computerized-numerical-controls

Mitsubishi Electric M700 Series CNCs

We have produced high-performance CNC systems since 1973 and are the largest supplier of customized CNC systems for machine tool builders worldwide. Today we have more than 100,000 CNC systems in operation throughout North America.

jrmachinelogo

JR Machine

  • Founded: 1992
  • Business: JR Machine is a leading contract manufacturing company for complex precision machined parts.

Return to Case Studies