-
Inquiries
-
Select
& Quote -
Share
-
Partners
Webcasts On-Demand
Built-In PLC: The Evolution in VFD Performance and Intelligence
Aug 28, 2020 - Webcast
Distributed control with variable frequency drive technology is here today! The FR-E800 Series VFDs combine motor control and process control into one automation unit with added input/output signal and logic, and the processing power of a built-in PLC.
The webinar will cover:
- The ability to have distributed control without added automation equipment
- Ladder or structured programming with functions blocks for ease of use
- Inverter-to-inverter communications made possible with built-in PLC control