fa_logo

Webcasts On-Demand

Improve Machine Reliability with Servo Based Maintenance

mini_hero_banner

Jun 12, 2020 - Webcast

High machine reliability is a choice and not an accident of fortune. A plant’s productivity is influenced by individual machine reliability, which is in turn evaluated by mechanical component performance. To improve machine reliability, Mitsubishi Electric's servo based maintenance prevents machine unplanned shutdown, schedules routine maintenance, and reduces the turnaround process. The patented predictive maintenance function is integrated in the MELSERVO-J5 amplifier, which utilizes artificial intelligence and state of the art machine diagnosis.


Return to Webcasts On-Demand List