Programmable Sewing Machines

SEWING_MACHINE_290x215_RoundedCorners

The current PLK-J Series machine is the sixth generation of the PLK. It uses 2 upper and lower servos and 5 stepping motors digitally connected to eliminate mechanical shafts and connecting linkage. Main features include digital tension, presser foot motion, material thickness detection, newly designed X/Y motion and much more. For e-F@ctory solutions, Ethernet connectivity to support factory automation products is possible. All sewing parts and electronic components are available.

PLK-J Series

The current PLK-J Series machine is the sixth generation of the PLK. This next generation PLK-J series represents the latest in mechanical design, newly added features, and functions. Traceability through factory added material ply detection, skipped stitch detection, and digital tension are standard on large area machines. Ethernet connectivity allows an easy connection for other Mitsubishi Electric factory automated products for production and maintenance management.

SEWING MACHINEBackground_290x215

PLK-G Series

The current PLK-G Series machine is the fifth generation of the PLK. It uses USB memory for pattern storage as well as an internal memory. The machines are equipped with an on-board touch screen for making sewing patterns and customizing parameters. All sewing parts and electronic components are available.

PLK-G

PLK-E Series

The previous PLK-E Series machine was the fourth generation of the PLK. It uses a standard floppy disk for pattern memory as well as an internal memory. The machines are equipped with an on-board touch screen for making sewing patterns and customizing parameters. All sewing parts and electronic components are available.

PLK-E

PLK-B Series

The previous PLK-B Series machine was the third generation PLK. It uses a standard floppy disk for pattern memory as well as an internal memory. The machine was designed with the option of an on-board programmer for making sewing patterns. All sewing parts and electronic components are available.

PLK-B

PLK-A Series

The previous PLK-A Series machine was the second generation PLK. It uses a standard floppy disk for pattern memory with an on-board programmer for making sewing patterns. Main sewing parts are available. Electronic components are no longer available.

PLK-A

PLK Series

The previous PLK Series machine was the first generation of the PLK and used an e-prom for pattern memory. It did not option the ability to make a sewing pattern on the machine. Main sewing parts are available. Electronic components are no longer available.

PLK

How Can We Help You?
Automation
Contact Sales
Get Quote
Join Us
Contact Support
Connect With Us
Facebook44 LinkedIn44 Twitter44 YouTube44 instagramlogo44