fa_logo

Class Offerings

Operator Interfaces (HMI)

mini_hero_banner
Gain cutting-edge skills with our operator interfaces (HMI) training programs.

Our classes are designed to develop students' understanding of the Mitsubishi Electric family of graphical operator terminals. They include topics such as the features of operation and the software needed to create, configure and modify screens.

Operator Interfaces (HMI) Training
 

GT Designer3 Programming (TRHMI102P)

This course familiarizes attendees with the GOT2000 and GOT3000 family of operator interface products and the software needed to create, configure and modify screens which can be used with PLC systems.