fa_logo

Virtual Training

GT Designer3 Programming

mini_hero_banner

GT Designer3 Programming Training

GT Designer3 Programming virtual training

This course is intended to familiarize the student with the GOT2000 and GOT3000 family of operator interfaces and the GT Works3 software used to create, configure, and modify screens. This virtual course will be taught using the simulation functions of GT Works3 and will cover the various models of GOT2000 and GOT3000, creating a project, configuring basic screen objects, and transferring the project to the operator interface terminal.

Course requirements: For this course we require basic experience using GX Works3. It is highly recommended that the student is familiar with controller programming and troubleshooting.

Optional

Course materials:

  • No hardware needed.
  • GX Works3 and GT Works3 software (If you do not have the software, a free 30-day trial version can be provided for the class).

Course duration: This course will be taught in 3 consecutive half-day sessions.

Interested in Registering for this Virtual Training?