-
Inquiries
-
Select
& Quote -
Share
-
Partners
FR-D800 Series VFDs
Peripheral Software
- Feature
- Specification
- Standards
- Discontinued
FR Configurator2 - Simple parameterization, troubleshooting and monitoring
FR Configurator2 is user-friendly software that simplifies everything from setup to maintenance, offering many powerful functions.
Free trial versionsupported
The function is available in the free trial version (usable free of charge with limited functions).
| Function | Free trial version |
|---|---|
| Parameter list | ○ |
| Diagnosis | ○ |
| AI fault diagnosis | × |
| Graph | × |
| Batch monitor | × |
| Test operation | ○ |
| I/O terminal monitor | × |
| Function | Free trial version |
|---|---|
| Convert | ○ |
| Developer | × |
| USB memory parameter copy file edit |
× |
| Help | ○ |
○: Available ×: Not available
| Function | Free trial version |
|---|---|
| Parameter list | ○ |
| Diagnosis | ○ |
| AI fault diagnosis | × |
| Graph | × |
| Batch monitor | × |
| Test operation | ○ |
| I/O terminal monitor | × |
| Convert | ○ |
| Developer | × |
| USB memory parameter copy file edit |
× |
| Help | ○ |
○: Available ×: Not available
The trial version (usable for a limited period), for which all the functions of the product are available for 30 days, is also provided.
Life diagnosis check
Parts service life data is displayed in a dedicated window.
An alert icon is shown in the parts life alarm field for the parts recommended for replacement. This can be used as a guideline to replace long life parts.
Graph function and trace function
Waveform graph data immediately before the protective function is activated can be automatically obtained. Graph display and log analysis are available using the stored trace data.
Sophisticated motor & VFD sizing with Motorizer selection softwareTo be supported</sup>
Users can select motors by entering data of mechanical configuration, specifications, and operating patterns. Applicable combinations include VFDs, sensorless servo drive units, and AC servo amplifiers. The most suitable combination can be selected from the selection result. The software also supports multi-axis systems.
Twelve types of load mechanism such as a ball screw or a rack and pinion are selectable. Selection is available by following the steps from 1 to 3.
When users include the power regeneration common converter or other applicable converter, the capacity of the converter can be selected at the same time.
Click here for details Drive System Sizing Software Motorizer
Advanced system design and selection with FA Integrated Selection Tool
Select VFDs, accessories, and create networks topology along with complete bills of materials.
Click here for details FA Integrated Selection Tool
Quickly visualize VFD data with GOT (HMI) Functions <sup>To be supported</sup>
Enhanced compatibility between VFDs and the GOT (human machine interface) brings various benefits to users.
Connection with the GOT2000 series can be established just by setting the station number.
Other necessary settings are automatically done.
-
STEP 1
Select the GOT and the VFD and connect them.
-
STEP 2
Sample screens for selected connection type available to be imported to user's project data.
-
STEP 3
Transfer the project data to the GOT.
Improving work efficiency without using a computer
Users can use the GOT to set up, adjust, and perform maintenance for VFDs without using a computer.
Immediate warning of system errors
By storing the data of relationship between the output frequency and the torque during normal VFD operation, users can judge whether the load is operating in normal condition. By outputting out-of-range warnings if applicable, users can detect mechanical faults or perform maintenance.
Reducing downtime by interacting with the GOT
Faults occurred in the VFD can be displayed on the GOT screen.
When a fault occurs, it is possible to identify the fault details immediately, which contributes to downtime reduction.