-
Inquiries
-
Select
& Quote -
Share
-
Partners
FR-D800 Series VFDs
Reduced downtime
- Feature
- Specification
- Standards
- Discontinued
Quickly resolve issues with effective diagnostic tools
Troubleshooting support tool
FR Configurator2
- Graph function
Utilize high-speed sampling to graphically display VFD data, improving analysis of problems and identification of root causes.
- Trace functionNEW
VFD stores critical operating data like DC Bus voltage from the moments before a drive fault. The data can be uploaded for evaluation in a graphical format or shared with others. This enables a quick evaluation of the fault and rapid resolution.
Simple Upgrade from previous VFD models
FR Configurator2 (Convert function)
The parameter settings of the FR-D700 and FR-F700PJ (to be supported in April 2026) can be converted to FR-D800 parameters using FR Configurator2, simplifying replacement.
Input terminal filter
Input Filter (debouncing) smooths the input signal to ensure reliable operation of the VFD.
Easy wiring
Spring clamp terminals
Spring clamp terminals have been adopted for control circuit terminals for easy wiring.
Operate during and/or recover from external challenges
Emergency drive (Fire mode) NEW
For critical operations during emergencies like a fire, the VFD can operate the motor, even if faults are detected, overriding protective functions.
- *: This function is disabled in the initial status. To enable this function, set Pr.523 (Emergency drive mode selection).
- *: Use of this function may damage the motor or VFD.
Use this function for emergency operation only.
The operation can be switched to the commercial power supply operation at the occurrence of a fault which may cause damage of the inverter.
Air handling system
Automatic restart after instantaneous power failure function
After an instantaneous power failure, the motor speed is detected upon power restoration, enabling a smooth restart from the coasting motor speed.
Power failure time deceleration-to-stop function
In the event of an instantaneous power failure or undervoltage, the motor can be decelerated or decelerated to a stop, and reaccelerated to the set frequency upon power restoration.
This avoids the danger caused by coasting during a power failure.
This function is effective for grinders with large inertia.