fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Hardware Features

Design secure network configuration
Ethernet communication unit

Having problems?

Having problems?

I want to separate the network for security reason.

GOT will solve your problems!

GOT will solve your problems!

Two Ethernet ports physically separate the information system network in the office from the control system network at the shop floor; therefore the network architecture is more reliable and secure.

  • *Installation of the Ethernet communication unit (GT25-J71E71-100) is required on the GOT.
  • *GT25 wide and GT25 rugged models have two Ethernet ports as standard so that the Ethernet communication unit is not required.
  • *Not supported by GT2505 and GT25 handy because the Ethernet communication unit cannot be installed on these models.

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●To use Ethernet communication unit

To use the Ethernet communication unit, the BootOS version Z or later is required. Because the unit cannot be used depending on the connection destination, please refer to the GOT2000 Series Connection Manual.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25* GT23 GT21 GS21 SoftGOT
  • *Excluding some models. For the details, refer to the function descriptions above.

Related Links

banner_selection_tool_en