fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Video Interactive Solutions

Monitor shop floor using video images
Video display/RGB display/Video output function

Having problems?

Having problems?

There is not enough space for multiple monitors at the shop floor.

GOT will solve your problems!

GOT will solve your problems!

GOT acts as a monitor to display images which are recorded by a video camera or saved in a personal computer, and thus there is no need to have additional monitors.

Function features

GOT acts as a monitor to display images which are recorded by a video camera or saved in a personal computer.

Video input*1

Input images of up to 4 video cameras can be simultaneously displayed on the GOT. You can zoom in or zoom out the images and save the GOT images (hard copy images).

RGB input*2

RGB images can be displayed on the GOT. Simultaneous display of two screens is also possible*3. You can use various effects for the images such as rotation, and gesture operations can be used for zooming in/out (400%) and scrolling objects*3.

RGB output*4

The GOT screen can be displayed on a commercially available large display even when the backlight of the GOT is off.

HDMI output*5

Connect an HDMI compatible monitor and display GOT screens on the large monitor. Since the GOT screen can be displayed on a large monitor, it is recommended for ANDON applications.

Different screens can be displayed on GOT and an external display by using the RGB output unit or the digital video output unit.
  • *1Video input unit (GT27-V4-Z) or video/RGB input unit (GT27-V4R1-Z) is required.
  • *2RGB input unit (GT27-R2) or video/RGB input unit (GT27-V4R1-Z) is required.
  • *3Supported by GT27-R2 only.
  • *4RGB output unit (GT27-ROUT) is required.
  • *5Digital video output unit (GT27-VHOUT) is required.

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●Unit installation

One of the following units can be installed: multimedia unit, video input unit, digital video output unit, RGB input unit, video/RGB input unit, RGB output unit

●Applicable peripheral devices

For the details, please refer to the Technical Bulletin No. GOT-A-0160-AE (PDF).

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27* GT25 GT23 GT21 GS21 SoftGOT
  • *Excluding GT2705.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en