fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Startup/adjustment

Parameter recipe (simple backup/restoration)

  • CASE1
  • CASE2
  • CASE3
  • CASE4
  • CASE5
GT27 GT25 GT23*2 GT21*2 GS21*2 SoftGOT*2*3

Challenge

We want to return the parameters to the pre-adjustment values!

Challenge

What were the pre-adjustment parameter values...

Solutions

GOT Drive solves your problems

Back up/restore the pre-adjustment parameters with the GOT
The current inverter parameters can be backed up (saved) as a recipe file using the GOT. To return the parameters to the pre-adjustment state while starting up and adjusting the inverter, just restore (write) the parameters that were previously backed up (saved).

Solutions
  • *1Sample screens (VGA) are available. The screen image is the sample screen of FR-A800-E for CASE 1. The screen image differs from the one for FR-E800. The sample screen of this function is not available for FR-E700/FR-D700 in CASE 4.
  • *2Sample screens are not supported by GT23, GT21, GS21, and GT SoftGOT2000.
  • *3Supported by GT SoftGOT2000 (Multiple channels) only.

Related Links

banner_selection_tool_en