fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Startup/adjustment

FA transparent

  • CASE1
  • CASE2
  • CASE3
  • CASE4
  • CASE5
GT27 GT25 GT23 GT21 GS21 SoftGOT

Challenge

We want to perform debugging smoothly!

Challenge

Solutions

GOT Drive solves your problems

Debugging via GOT without opening the control panel
By connecting a personal computer with the GOT's USB interface, the inverter can be programmed, started up, and adjusted via GOT. There is no need to open the control panel and change the cable.

Solutions
  • *1Some system configurations are not supported. For the details, please refer to the connection manual.
  • *2The wireless LAN communication unit (GT25-WLAN) needs to be installed on GOT. The unit cannot be used with GT2505, GT25 handy, GT23, GT21, and GS21 models. For the countries where the unit can be used and other details, please see here.

Related Links

banner_selection_tool_en