VIEW with ASSISTA
ASSISTA and the camera capture the target using the “RT VisualBox” auto-focus function.

"RT VisualBox" proprietary engineering tool
The vision camera focus adjustment and work registration can be configured simply by touching the screen. This means that you can use it even without special robot knowledge.

Mitsubishi Electric Vision Sensor In-Sight
The high-performance camera identifies the target and fixes position at high speed. Its compact size makes it ideal for attaching to the ASSISTA robot hand. This wire-saving type is equipped with PoE.
*Products may not be available in the region where you consider purchase. For details, please inquire at each company.
Model Name |
Manufacturer |
Inquiries
(as of April 2020) |
Comments |
In-Sight 8402M-363-50 |
COGNEX |
COGNEX |
- |
In-Sight 8402M-373-50 |
COGNEX |
COGNEX |
Supports PatMax RedLine®
PatMax RedLine® cannot be used in combination with RT VisualBox |