Blogs
Anti-Sway VFDs for Cranes: Keep Throughput High When Skilled Operators are Scarce
Summary: This blog explains how Mitsubishi Electric's FR-E800 VFDs use sensorless anti sway, infinite speed control, and built-in PLC capabilities to help cranes operate more safely and efficiently, especially when skilled operators are hard to find. It highlights how the technology reduces load swing, improves cycle times, minimizes wear, and simplifies commissioning for crane OEMs, distributors, and end users.
Skilled Labor Challenges
Across the crane and hoist industry, one theme keeps coming up in conversations with OEMs, distributors, and end users: experienced operators are harder to find, and the work keeps getting more demanding. As the talent gap widens, load sway becomes a bottleneck, slowing cycle times, increasing equipment wear, and creating risks for people on the floor.
That's exactly where Mitsubishi Electric's FR-E800 VFDs change the equation. These drives were designed to make crane motion safer, more predictable, and easier to operate. Even when your most seasoned operator isn’t the one holding the pendant.
Mitsubishi Electric's Smart Crane & Hoist Solution
FR‑E800 sensorless anti‑sway, infinite speed control, built‑in PLC
- Ideal for overhead crane applications and below (for higher load applications see FR-A800).
- Sensorless anti‑sway and sensorless positioning keep the rope near vertical for predictable stops and landings.
- Infinitely variable speed control gives operators fine control within safe limits.
- Built‑in PLC handles interlocks, brake sequencing, and auxiliary logic.
- Ethernet connectivity for diagnostics and easy integration.

How sensorless anti-sway works
The drive shapes acceleration and deceleration to align with the suspended load's natural frequency. Experienced operators often do this by feel, but anti-sway automates the process so motion stays smooth even with newer operators. For seasoned operators, it reduces the need for timing-based finesse and lets them stay focused on situational awareness, improving overall safety on the shop floor.
The simplest analogy: It's like carrying a cup of water.
If you stop abruptly, the water sloshes. If you move in a way that matches the slosh, you keep the water stable. Experienced operators learn this timing instinctively. Anti-sway applies that same logic automatically, so operators get smooth, predictable motion with much less skill required.
Whether the movement is manual or automated, the goal is the same: reduce the swing, speed up positioning, and maintain consistent operation.
Key Takeaways
If it’s getting harder to find experienced operators, your control system can bridge that gap. With sensorless anti sway, infinite speed control, and built in PLC capability, the FR-E800 helps OEMs and operators with:
Quicker installation, configuration, and commissioning
- Crane and hoist features with simple configuration accelerate setup time across hoist, trolley, & bridge.
- Built‑in PLC simplifies control architecture.
- Standardized drive profiles across axes and crane sizes reduce startup time.
- Tested under extreme conditions and backed by our 5-year warranty.
Performance making a valuable impact
- Faster training and consistent cycle times mean less reliance on one expert.
- Lower maintenance due to smoother ramps, reducing brake shock, wheel/rail wear, and skew.
- Reliable modernization path for aging cranes and new designs.
Proven in the Field
Customers are having success using our Mitsubishi Electric Crane and Hoist VFD solutions. See our collection of success stories here.
Interested in trying out the anti-sway technology for yourself? Test your skills with our Anti-Sway Crane game.
Want notifications for new Blogs, White Papers, Case Studies & Webinars?
Contributors
Benjamin Strong
Industry Marketing Manager (Drive Systems)
Mitsubishi Electric Automation, Inc.
-
Inquiries
-
Select
& Quote -
Share
-
Partners