fa_logo

Case Study

IKA Technology

case_study_mini_hero
Download PDFPDF
IKA Technology implements robot vision system to provide safety for employees and achieve time-savings

First released December, 2024

Key Points:

  • 1. The Challenge: Automate a time-consuming and safety-lacking process
  • 2. The Solution: 4-axis robot with added vision and intelligence
  • 3. The Result: Significant safety, cost savings, and time saving benefits

The Challenge - Automate a time-consuming and safety-lacking process

Spectrometry is a micro-analytical technique used to identify and quantify compounds within molecules. These processes are usually associated with the food and beverage industry, water treatment, and environmental quality control.

However, IKA Technology, a Diamond Partner Systems Integrator of Mitsubishi Electric Automation, sought to automate tasks in the spectrometry process to measure the purity of metals.

Spectrometry

The end-user, Helmut Fischer, sought a solution for their current, manual metal measurement process. According to Jose Antonio Diaz, Business Developer at Helmut Fischer, the manual nature of the process made it time-consuming to evaluate the pieces, and they could not assay the required volume of pieces entirely. In addition, requiring a worker to perform the process manually was potentially exposing them to harmful X-rays emitted by the measuring instrument. It was clear that an automated solution was required to ensure the safety of these tasks and that production rates would improve.

The Solution - 4-axis robot with added vision and intelligence

IKA Technology decided to assemble a multidisciplinary team with experts in various areas and from various organizations to deliver the best solution to the end user.

They agreed that to achieve the intended goal, they must integrate a 4-axis robot, a vision system, a conveyor belt, and the instrument that will perform the spectrometry.

4 Axis Robot with Vision

From that premise, Dr. Eduardo López, an expert in vision, proposed implementing an artificial vision camera. This camera would analyze each piece of metal regardless of weight and/or size. This would allow the robot to place it in the precise location for the next step of the process, where measurement could be performed.

Victor Quote2

"A project of this nature requires high specialization in different areas such as robotics, machine vision, and material analysis. Mitsubishi Electric is the only brand that provides us with this level of integration."

- Dr. Víctor Eduardo López
Robotics and Vision Expert

Jonathan Granados, a PLC and Robot Programming Engineer at IKA Technology determined that since the process is highly repetitive, the belt should not be in constant motion. A direct drive would increase energy consumption, so to save energy, Jonathan proposed using VFDs to modulate the speed and start/stop of the metals on the belt.

To meet the application's requirements, the team connected a SCARA-type robot, an Industrial PC that receives data from the vision system, a couple of microinverters, and low-voltage devices. For this, the team selected the iQ-F Series FX5U PLC from Mitsubishi Electric because it has straightforward discrete control, supports several simultaneous communications in different protocols, and can control multiple smart devices since all the cell's equipment responds to this master controller.

FX5U

The team then selected FR-D700 Series VFDs with vector control to enhance torque response and increase the motors’ efficiency by incorporating optimum excitation control, which can result in up to 20% energy savings. Additionally, being compact, the VFDs have bookshelf mounting capability, reducing the total installation space within the cabinet, which will cut the overall cost of the installation.

IKA Technology Case Study Video

The Result - Significant safety, cost savings, and time saving benefits

Metal pieces are placed randomly on sample racks and enter the process via the conveyor belt, where the inverters are responsible for modulating the required speed variations to manage energy consumption.

Jonathan Quote

"By choosing equipment that speaks the same communication language, you make the project's programming and implementation flow much more smooth."

- Jonathan Granados
IKA Technology

The robot then picks up the piece and places it under the artificial vision device, which collects dimension and position data. Subsequently, the robot will place it on the measuring instrument, which will yield a result of GOOD (OK) or NOT GOOD (NG). The PLC will then instruct the robot whether this piece should proceed to the next stage of the process or be discarded. Finally, if the measurement result is good, the robot will place the piece on the final line of the process and pick up a new piece.

Through this process, the end user will obtain precise data about the purity of each piece in less time, saving energy and without the risk of exposing the operator to the X-rays that could have happened with the manual process.

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

scara-robots

MELFA RH Series SCADA Robots

Designed to work in a diverse range of high-speed applications, the RH (horizontal type) SCARA robots are ready to be the high speed robotic solution for even the most demanding of applications.

d700-e800

FR-E800 and FR-D700 Inverters (VFD)

Mitsubishi Electric delivers innovative, open, flexible and reliable VFD solutions geared to the special needs of individual markets and customers.

fx5u

MELSEC iQ-F Series Programmable Controllers

From stand-alone use to networked system applications, the MELSEC iQ-F series brings your business to the next level of industry.

ikalogo

IKA Technology

  • Business: Experts in automation and industrial control, manufacturers of control panels and marketers of leading brands in the automation industry.

Return to Case Studies