fa_logo

Case Study

Rocheleau Tool’s Blow Molding Machines “Only Have to Run Forever”

mini_hero_banner
Download PDFPDF
rocheleau-banner

First Released December, 2020

Rocheleau, a blow molding machine OEM out of Massachusetts, has a company motto: “fear no task”. It goes back four generations for the Rocheleau family, and it’s not just a statement. It’s a challenge: to innovate and make better products that bring new benefits to customers. And since the 1980s, Mitsubishi Electric has been their trusted partner.

Fear No Task

The company motto – Fear No Task – goes back four generations for the Rocheleau family. For them, it’s not just a statement. It’s a challenge: to innovate and make better products that bring new benefits to customers. As one of the top manufacturers of blow molding machines for the plastics and packaging industry, this motto has served them well.

Another thing that’s served them well? When they find a provider that consistently delivers the highest quality products, they tend to stick with them.

Rocheleau has been using Mitsubishi Electric controls exclusively since they moved from relay logic systems to programmable logic controllers (PLCs) in the late 1980s. Mitsubishi Electric controls are in every piece of equipment they produce. And they reliably control every aspect of operation:

  • Motors
  • Temperature
  • Pneumatics
  • Hydraulics
  • And more

Kevin Hastings, Electrical Engineering Manager, 3rd Generation Co-Owner, and grandson of Rocheleau’s founder, says controls are like tires on a car. “No matter how well you build the car, if you have a flat tire it’s not going to drive down the street.” Kevin says, “Controls are even more important to machines than tires are to cars. If they break down, nothing is going to work at all.”

Quote

“Mitsubishi Electric products have proven to be extremely reliable and help us ensure that our equipment will keep on working as intended—and that our customers will keep on getting trouble-free operation.”

- Kevin Hastings, Electrical Engineering Manager
Rocheleau

If you drink juice or milk, put sugar in your coffee, use household cleaning or personal care products, you’ve probably used one of the containers created on Rocheleau machines. And these containers are created incredibly fast — especially when they are created on Rocheleau’s flagship machine: the RS-90 extrusion blow molding machine.

The Next Generation of Efficiency, Power and Speed

Rocheleau introduced its next-generation extrusion blow molding machine at the same time they celebrated their 80th year in business. This first-ever 6-head, 1-gallon blow molding machine fills a need in high-volume packing applications. It tackles tubs and larger bottles at significantly faster cycle times. How fast? It runs a six-cavity high-density polyethylene gallon in the mid six seconds range.

ROCHELEAU Case Study

Mitsubishi Electric’s iQ-R Series PLCs ensure high productivity and consistent product quality.

Quality You Can Count On

On a handful of occasions, a customer for whatever reason asked Rocheleau to build a machine using a different brand of controls. Fortunately, in each case Kevin was able to talk them out of it. And the customers loved the machines and ordered more. The question of using different controls never came up again.

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

iq-r-series-programmable-logic-controllers

iQ-R Series PLCs

MELSEC iQ-R Series: As the core for next-generation automation environments, Mitsubishi Electric has created an automation controller with added value while reducing TCO.

got2000-series-human-machine-interfaces

HMIs

The GOT2000 Series HMI provides a range of models to fit a variety of performance and screen size requirements. All models provide advanced features that improve operator efficiency and performance.

fr-d700-variable-frequency-drives

FR-D700 VFDs

FR-D700 is Mitsubishi Electric’s class-leading range of micro drives. Suitable for a wide variety of general purpose motor speed control applications, the FR-D700 was built from the ground up using custom components and has earned an enviable reputation for durability and dependability in adverse environments.

logoquote291x489

Rocheleau Tool

  • Founded: 1938
  • Business: ROCHELEAU designs, builds, services, and operates highly productive and efficient blow molding machinery that is simple in design and exceptionally versatile.

Return to Case Studies