News Center
Press Releases
Introducing LoadMate Plus™ Robot Cell for Flexible Machine Tool Tending
Vernon Hills, Illinois - April 19, 2021
Mitsubishi Electric Automation, Inc. is announcing the release of its LoadMate Plus engineered solution. LoadMate Plus is a robot cell which can be easily moved for efficient use, and is targeted towards manufacturers in CNC machine tool applications that find themselves facing a labor crunch, while needing to be more efficient and improve their production. The robot cell provides flexible solutions for traditionally high-mix, low-volume facilities to introduce automation, and is designed with mobility and flexibility in mind.
LoadMate Plus automates the task of loading and removing parts from a machine tool through the use of robotics, and can be mounted next to one machine, between two machines, and otherwise moved around a facility as jobs require. When this cell is paired with Mitsubishi Electric M8 Series CNC, operators can use the Direct Robot Control (DRC) feature within the CNC controls to also control and program the robot with menus and G-code from the same screen used for the machine tool. No robot programming experience or teach pendant is required, allowing manufacturers to use existing staff to automate and make adjustments.
“Most automation solutions for machine tending rely on either cobots for flexibility, or industrial robots for performance and larger parts,” said Rob Brodecki, services product manager at Mitsubishi Electric Automation. “With LoadMate Plus, users don’t have to sacrifice one for the other. The cell is flexible, regardless of the robot, and users can choose from a number of robots to match a shop’s specific needs. Plus, with an available 3-year robot warranty, and Mitsubishi Electric technicians who can service LoadMate Plus, users can ensure that their production will continue uninterrupted.”
More Information
- About Mitsubishi Electric US, Inc., Industrial Automation Division
Headquartered in Vernon Hills, Ill., Mitsubishi Electric US, Inc., Industrial Automation Division provides a comprehensive portfolio of industrial automation solutions. Offerings include programmable automation controllers (PAC), programmable logic controllers (PLC), human machine interfaces (HMI), variable frequency drives (VFD), servo amplifiers and motors, control software, computerized numerical controllers (CNC), motion controllers, robots and low-voltage power distribution products. Additional information about Mitsubishi Electric US, Inc., Industrial Automation Division is available at us.mitsubishielectric.com/fa/en/.
- About Mitsubishi Electric US, Inc.
Headquartered in Cypress, CA, Mitsubishi Electric US, Inc., a US affiliate company of Mitsubishi Electric Corporation, supports US innovation initiatives and currently provides cooling and heating solutions, elevators and escalators, space and sensing systems, semiconductor devices, and industrial automation. Mitsubishi Electric contributes to a vibrant and sustainable society through continuous innovation and making "Changes for the Better." For additional information, visit .
- Media Contact
Pam Summers
Marketing Communications Manager
Mitsubishi Electric US, Inc., Industrial Automation Division
Pam.Summers@meau.com
+1 (847) 478-2415
-
Inquiries
-
Select
& Quote -
Share
-
Partners