fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Security & Additional System Features

More information on a single screen
Base screen size expansion

Having problems?

Having problems?

Can I check all necessary information on one screen without switching screens?

GOT will solve your problems!

GOT will solve your problems!

A base screen that is larger than the resolution of GOT can be created and displayed. By displaying the information that used to be separated in multiple base screens, operation can be performed while viewing the whole image.

Function features

A base screen that is larger than the resolution of GOT can be created and displayed. The screen of expanded size can easily be scrolled by using swipe gestures or the scroll bars.

*Supported by GT SoftGOT2000 only when using the SoftGOT-GOT link function.

Example)
Displaying an expanded base screen (1600 × 960) on GT27-V (640 × 480)

Example) Displaying an expanded base screen (1600 × 960) on GT27-V (640 × 480)

Always display overlap window

Even if the screen is scrolled, the overlap window on the GOT screen is kept displayed in the same position. If there are some objects or information that always need to be displayed on the screen (function keys, etc.), it is possible by using an overlap window.

Operation while viewing the whole image

The navigation window can be displayed on GOT to indicate the current position on the base screen. The window is semitransparent and displayed in small size to help you view the whole image during operation.
The window display can be changed depending on the setting (always display, do not display, or display while swiping/ touching the screen).

Operation while viewing the whole image

Specification details and restrictions

●Graphics setting

GOT Graphic Ver.2 must be selected.

●Restrictions of other functions

This function cannot be used with the screen gesture function.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21 GS21 SoftGOT*

*Restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en