fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Security & Additional System Features

Support recipe setting (record) selection
Recipe display (record list)

Having problems?

Having problems?

How can I change recipes easily on a user-created screen?

GOT will solve your problems!

GOT will solve your problems!

Recipe names (record names) are displayed in a list format on GOT. Sort or narrow down the list and easily change recipes on GOT.

Function features

Create the recipe display (record list) easily just by selecting required items in GT Works3. Colors, line styles, and borders can be changed as you need.

Read and write records

Just select a record and touch a switch on GOT and you can easily read or write records.

Change display order of records

Records can be sorted by record number or record name by touching the column header.

Change or delete record names

Change record names or delete records by specifying the record name using text input.

Specification details and restrictions

●Customizable settings

Text color, background color, cursor color, ruled line color, line type, line width, show/hide scrollbar, etc.

●Functions that can be used with recipe display (record list) object

Read/write records, delete records, verify records, change/sort/filter record names, export/import recipe data

●How to obtain sample screens

Sample screens are included in GT Works3. For the details, please contact your local sales office.
The sample screens are supported by the following GT Works3 versions: Ver.1.155M or later.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21 GS21 SoftGOT

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en