fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Security & Additional System Features

Security with password management
Operator authentication function

Having problems?

Having problems?

How can I restrict the unauthorized operators?

GOT will solve your problems!

GOT will solve your problems!

Operator name and password enable the secure login management in a large-scale shop floor, providing the flexibility of setting the operation authority per shop floor or operator. In addition, the login management can be performed by an external authentication device such as RFID.

Function features

Setting the operation authority and the viewing authority achieves "enhanced security" and allows "access management per operator". Use of the operator authentication function combined with the operation log function enables you to check the "who, what, when, and how" of an operation performed.

Enhanced password security

By setting password requirements (the minimum number of characters and the character types), you can set more advanced passwords. It is possible to prompt a password change at the initial login or notify the password expiration date in advance (1 day to 30 days). In addition, supported the function to prohibit the setting of passwords that were used in the past.

*Not supported by GT21 and GS21.

How to authenticate the operator

Use of method ① combined with method ② is acceptable. Secure login management is achieved even when an external authentication device has failed.

Method① Input an operator name and password for login: Method②Use an ID card or ID tag for login

Settings for operation authority

Set the authority to allow John Smith to adjust "Torque 1" and "Torque 2".

John Smith can adjust

*For the necessary option devices, please refer to the "Function list".

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21* GS21* SoftGOT

*Restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en