fa_logo

Human-Machine Interfaces(HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

Interactive Features with Other Industrial Devices

Support CNC maintenance
Interaction function with CNCs
Support maintenance work

Having problems?

Having problems?

"NC alarm" occurred on a GOT!
How can I maintain the system quickly?

GOT will solve your problems!

GOT will solve your problems!

Use a GOT to monitor or check alarms of a CNC. When an NC alarm occurs, there's no need to use a personal computer when modifying programs and you can quickly recover the system.

Function features

A GOT can be used to display various monitors and make settings of a CNC connected to the GOT.

CNC monitor 2 function (CNC C80)*1

The function enables monitoring and operation of the standard screens (monitor, setup, edit, diagnosis, and maintenance) of the C80 Series CNC connected to the GOT. You can also use this function to input/output data or edit machining program of the CNC C80.

CNC monitor function (CNC C70)*2*3

The function enables the alarm diagnosis, position display monitor, tool compensation/parameter setting, or program monitor of a CNC C70 connected to the GOT.

CNC machining program edit function (CNC C70)*2*3

Machining programs and MDI programs of a CNC C70 connected with the GOT can be edited.

CNC data I/O function (CNC C70)*2*3

Machining programs and parameters can be copied, compared, or deleted in a CNC C70 connected with the GOT.

CNC data I/O function
  • *1Not supported by GT25 wide and GT25 rugged models.
  • *2Supported by GOTs with a resolution of SVGA or higher.
  • *3Not supported by GT25 wide, GT25 rugged, and GT25 handy models.

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●Target models

CNC(C80、C70)

●Supported connection types

Ethernet connection (DISPLAY I/F connection only)*1, bus connection*2

  • *1The CNC data I/O function cannot be used with CNC C70 when CC-Link IE Field Network Ethernet adapter module is used.
  • *2Supported by CNC C70 only.

●Target data

CNC monitor 2 function
The target data is the same as that of the CNC monitor function, the CNC machining program edit function, and the CNC data I/O function.

CNC monitor function
Alarm diagnosis, position display, tool compensation/parameter setting, program

CNC machining program edit function
Machining program, MDI program

CNC data I/O function
Machining program, parameter, tool offset data, workpiece offset data, common variable, maintenance data, cycle monitor data

Recommended industries

Automotive Electronics

Supported GOT types

GT27* GT25* GT23 GT21 GS21 SoftGOT
  • *Excluding some models. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en