fa_logo

Case Study

T-ROC Equipment improves made-to-measure box system with Mitsubishi Electric Automation solution

mini_hero_banner
Download PDFPDF
troc-equipment-banner

First Released March, 2019

Learn how Mitsubishi Electric products helped T-ROC Equipment, a box machine manufacturer, automate their process, increasing efficiency, reducing waste, and saving a significant amount in shipping costs.

BACKGROUND

T-ROC Equipment, a Kansas City, KS based box machine manufacturer built the very first state-of-the-art, heavy duty, automated box making machine in 1995. T-ROC is changing the face of the packaging industry by creating high quality machinery designed to help companies improve their bottom line in a multitude of ways. Most importantly, by improving shipping efficiencies and carrier costs for their customers.

CHALLENGE

T-ROC serves customers with varied box requirements. With the saturation of e-commerce as a primary commercial distribution model, T-ROC customers are now faced with shipping costs based on package size and weight. Box sizing has never been more important in improving profitability. Identifying the customer’s optimum box size can produce dramatic reductions in shipping costs. As a complete solution for box making, T-ROC needed an easy to use and automatic way of measuring the items to be boxed, sometimes in lot sizes of one, and capable of loading the appropriate dimensions into the board feeder and box maker.

kmV Logo

“The Mitsubishi iQ-F PLC was the exact fit for our control needs on the Automated Box Sizer and helped us meet our customer’s needs within their budget..”

- Ron Cowell, Owner, CEO
T-ROC Equipment

SOLUTION

On semi-automatic box machines, to make a box or inner packaging, an operator must select an icon that represents a box blank style. The HMI leads the operator step-by-step, through the entire process of choosing dimensions, quantity, and tabs for every style. Long containers for extrusions, folders for books, dividers, pads, or standard boxes, can be selected. The touch screen automatically prompts when to start feeding sheets of material. Excess board, trimmed off during production, can be reused to make additional boxes, and environmentally friendly inner packaging, from such corrugated excess board, can be produced quickly.

With the new automated box sizer, items to be packed are set upon a sizing table and scanned with a mini array scanner which feeds an iQ-F series PLC capable of highspeed calculations. With engineering expertise, system programming, and application support provided by Power Motion, a value added Diamond Partner, to engineer the machine system, the successful machine is controlled by an FX5 controller and 2 axes of servo communicating via RS-485 to Banner Arrays. High-speed inputs are used for an encoder to measure height, Banner Array outputs wired to high speed interrupt inputs to tell the PLC when no beams were blocked and to record encoder count. The GOT uses the MES option to send the size and weight of the required box to the user SQL database where they are compared to common shipping carrier’s rates. This allows the user to custom box items in order to pack efficiently and ship as inexpensively as possible.

TROCHMI

TROCHMI

The OEM ultimately chose Mitsubishi Electric because of the supplier’s respected reputation in the industry, and customers have been excited with the ease and efficiency of the system. Wireless communication from the sizer to the box machine allows for flexible placement and workflows.

Thanks to Mitsubishi Electric’s precision PLC and servo system, boxes can be quickly sized without manual guesswork, resulting in less wasted material. Most importantly, shipping cost analysis based on box size, weight, and delivery time is showing that right-sizing the box can save a significant amount in shipping costs.

TROCSizing
TROCBoxing

T-ROC Machine Benefits

  • Improved accuracy
  • Precise fit to measure packaging
  • Lower shipping costs for customers

Mitsubishi Electric Value-added Advantages

  • Mitsubishi Electric Value-added Advantages
  • High speed measuring and data transmission
  • SQL server interface

Become Our Next Success Story

Automating the World 3 Boxes Logo

Become Our Next Success Story!

We love our customers and the challenges they bring to us. We also like to let our customers shine by discussing how we worked together to solve their biggest challenges. If you have a challenge that needs to be solved and would like to be our next BIG success story, reach out to us and let's connect!

Product and Solutions

fx5-programmable-logic-controller

FX5 PLC

The Mitsubishi Electric MELSEC-F series has undergone many advancements, making way for the next generation MELSEC iQ-F Series, with enhanced high speed bus, expanded built-in functions, advanced SSCNET III/H support, and improved engineering environment with parameter settings in GX Works3 engineering software.

melservo-j4-servo-amplifiers

MELSERVO-J4 Series

MR-J4 family of products leverages cutting edge technology to provide a high functionality, high performance solution with the most flexible amplifier in the Mitsubishi Electric lineup.

gt27-human-machine-interface

GT27 Human Machine Interface

GThe GT27 Series is a top end graphical operator terminal which includes displays from 5.7" all the way to 15" with resolutions of XGA, SVGA and VGA depending on model selection.

mes-interface-it-module

MES Interface IT Information Module

The MES Interface IT allows organizations to standardize on a method of sharing information between the production environment and the enterprise IT systems.

troclogo

T-ROC Equipment

  • Founded: 1986
  • Business: T-ROC is a leader in the box making industry with over 500 machines installed and operating worldwide.  

Return to Case Studies