-
Inquiries
-
Build YourQuote
-
Share
-
Partners
MELSEC MX Controller MX-R model
Features - Reducing machine management cost
- Feature
- Specification
- Standards
- Discontinued
- Significantly reduce downtime with visibility into issues
- Record system-wide data over the network
- Easily review items that need attention by marking problem areas
- AI analysis instantly extracts differences in appearance and movement
- Root cause analysis made easy with coordination between tools
- Speed up program debugging and analysis
- AI-assisted root cause analysis
- Automatically generate network parameters
- Reduce maintenance time with automatic parameter distribution
- Easier troubleshooting reduces downtime
Significantly reduce downtime with visibility into issues
Achieve speedy root cause analysis through system-wide recording of operational status and extraction of anomalies using AI.
Record system-wide data over the networkNEW
Workpiece status and operation history are fully recorded along with control data from each equipment and machine before and
after a problem occurs.*1 View time-synchronized recorded waveform data, programs and video to easily identify the root cause.
This allows you to quickly and comprehensively investigate the cause and prevent problems from recurring.
Data is automatically recorded before and after a problem occurs and at the start of the facility cycle
Recording before and after a problem occurs
- ■Data is recorded for specified periods before and after a problem occurs, enabling efficient root cause analysis
- ■Data can be collected in sync with motion operation cycles
- ■Recorded data can be saved to a network drive
*1: Co-recording function will be supported in the future.
*2: A camera recorder module is required.
Easily review items that need attention by marking problem areasNEW
The vast amount of recorded data is narrowed down to the items that need attention, reducing the time and effort required to identify the root cause.
AI analysis instantly extracts differences in appearance and movementFuture support
GX VideoViewer Pro uses AI to automatically detect anomalies in video and adds log markers at points of deviation from normal
conditions.
This streamlines the process of pinpointing the cause of problems.
Root cause analysis made easy with coordination between toolsNEW
Even if the playback speed is changed, the timing between the video, program monitor, and device waveform data can be
maintained, each showing the target moment.
You can analyze from multiple perspectives while checking points of change.
Check the range affected by a device/label at a glance
You can check the range affected by a device/label at a glance, making it easy to perform integrated analysis.
Speed up program debugging and analysis
Easily identify problematic code using GX Works3 diagnostic function. Use the system monitor to check the module configuration and the error status of the system. View the event history to see errors and operations performed in the controller and motion in chronological order, including detailed error information, causes, and corrective actions.
Analyze both sequence and motion programs simultaneously
One-stop search and analysis are available even for large programs with many labels and structures.
Select data of interest (device or label) to visually display related data that affects changes in the selected data in a flow diagram.
You can jump from the flow diagram to the corresponding part of the program, making it easy to identify the cause.
AI-assisted root cause analysisNEW
Track device relationships that are not apparent in the program using AI. Efficiently debug issues where the program appears fine but the equipment stops without generating errors through AI-powered data flow analysis. For AI analysis, recording and logging files from normal operation of the equipment or machine are required.
Automatically generate network parameters
Simply connect the engineering software to the manager station and click a button on the screen to automatically detect the system configuration and generate network parameters. Even if the system configuration is changed, you can easily update the parameters with the same simple operation. This significantly reduces network setup time.
*1: Local stations will be supported in the future.
Reduce maintenance time with automatic parameter distribution
When a device is powered on or reconnected, parameters stored in the manager station are automatically distributed to the device.
Even after replacing a device, there is no need for individual parameter writing, ensuring a smooth and efficient replacement
process.
Easier troubleshooting reduces downtime
The location of a cable disconnection and error can be quickly found by visualizing the CC-Link IE TSN network system image in order of connection using the engineering software GX Works3. Since diagnostics information can be checked in real time, a network error due to an unexpected wiring change and module setting change can be quickly found, reducing downtime.