fa_logo

Human-Machine Interfaces (HMIs)-GOT

GOT2000 Series

img-mv-1-sm
  • Feature
  • Specification
  • Standards
  • Discontinued

What is realized with GT25 Handy GOT

A single GT25 Handy GOT can be used for several processes

With the connector conversion box (GT16H-CNB-42S), you can switch devices to operate according to the ID number of the connector conversion box.
This function is useful when performing maintenance on several processes in a single system.

A single GT25 Handy GOT can be used for several processes

ID number recognition function

Set the ID to each connector conversion box and connect the GT25 Handy GOT to a specific programmable controller.

  1. 1When the connector conversion box and the cable are connected, the ID number is acquired.
  2. 2The GT25 Handy GOT is connected to the programmable controller which has the IP address set to the acquired ID.
ID number recognition function

Effective utilization of existing systems

When replacing the GT14 Handy GOT with the GT2505 Handy GOT, or the GT16 Handy GOT with the GT2506 Handy GOT, you can use the cables and options as they are.
The switch positions and appearance are inherited from the former model. Various functions of the GOT2000 Series are available with keeping their operational feeling.

Effective utilization of existing systems

Operation style according to the usage

Holding in hand
Hanging on a wall

Related Links

banner_selection_tool_en