-
Inquiries
-
Build YourQuote
-
Share
-
Partners
Human Machine Interfaces MELHMI-GOT
GT SoftGOT
- Feature
- Specification
- Standards
- Discontinued
Contents
Operating Environment
| Item | Description |
|---|---|
| Personal computer | ・A personal computer that can run Windows ・MELIPC (MI3321G-W, MI3315G-W) |
| OS*1*2*3*4*5*6 |
・Microsoft Windows Server 2022 Standard (64-bit) *7 ・Microsoft Windows Server 2019 Standard (64-bit) *7 ・Microsoft Windows Server 2016 Standard (64-bit) *7 ・Microsoft Windows 11 Education (64-bit) *7 ・Microsoft Windows 11 Enterprise (64-bit) *7 ・Microsoft Windows 11 Pro (64-bit) *7 ・Microsoft Windows 11 Home (64-bit) *7 |
| CPU | Intel Core i3 (8th generation) or later |
| Memory | 8 GB or more recommended |
| Display | 9 inches or larger with a resolution of FWXGA (1366 dots x 768 dots) or higher |
| Hard disk space | ・For installation: 5 GB or more recommended ・For execution: 512 MB or more recommended |
| Display color | High color (16 bits) or more |
| Hardware | Network adapter |
| Other software | The following software is required to create the project data.
・GT Designer3 (GOT3000) Version1.400S or later The following software is required to connect with GX Simulator3.・GX Works3 Version1.105K or later The following software is required to connect with GX Simulator2.・GX Works2 Version1.621X or later The following software is required to connect with MT Simulator2.・MT Works2 Version1.189X or later The following software is required to use the OPC UA client connection.・GT OPC UA Client Setting Tool Version1.06G or later The following software is required to set Commander.・GT SoftGOT1000 Version3.64S or later ・GT SoftGOT2000 Version1.215Z or later The following software is required to connect with MELSOFT Mirror.・MELSOFT Mirror Version 1.000A or later |
- *1Administrator privileges are required when installing GT SoftGOT3000.
Administrator privileges are not required when using GT SoftGOT3000.
If another MELSOFT product is running with administrator privileges, also start GT SoftGOT3000 with administrator privileges. - *2The following Windows functions are not supported by GT SoftGOT3000.
Activating the application with Windows compatibility mode
Fast user switching
Changing the desktop theme (or font size)
Remote desktop
Setting the size of text and illustrations on the screen to any size other than [Small-100%] - *3Disable high-speed startup.
If enabled, GT SoftGOT3000 may not operate properly when the personal computer is shut down and then started. - *4Some digital pens are unusable.
- *5Operation is not supported in a virtual environment such as Hyper-V.
- *6The following lockdown features are not supported.
Unified Write Filter
Assigned Access
USB Filter
Layout Control
AppLocker
Shell Launcher - *7Use the same language version of Windows OS as that of GT SoftGOT3000.
Example: When using the English version of GT SoftGOT3000, use the English version of Windows OS.
[ Trademarks and registered trademarks ]
Microsoft and Windows are trademarks of the Microsoft group of companies.
Other product and company names are either trademarks or registered trademarks of their respective owners.